Section
 

Issue No. 1 - May 2000
testata
cover botton Editorial Notes
botton FLASH: the MEMORY of the MOMENT
Demand for Flash memory is rocketing and the technology is becoming increasingly pervasive. ST is responding with new manufacturing capacity, an aggressive technology roadmap and "advanced architecture" devices for applications in digital consumer markets.
botton THE WHOLE PICTURE
Unleashing the power of CMOS imaging technology in applications ranging from toys to biometrics and automotive systems.
botton CONVERGENCE ¥ CONNECTIVITY ¥ CONSUMERIZATION
The convergence of these markets and the subsequent multiplicity of applicatons presents great opportunities to companies with expertise in all three areas and serious challenges for those absent from one or more of them.
botton Around the World
A Glance at ST's operations in the United States and news from ST in Asia Pacific and in France.
  botton COOPERATING for COMMUNICATIONS
A look at two of ST's recent announcements with its customer and strategic partner, Alcatel.
  botton ALL YOU HAVE to DO is DREAM
Imagine a technology platform that could design a custom processor core optimized for your System-on-Chip application and also generate a complete software toolset automatically ! A system designer's dream ? ST and Hewlett-Packard's platform based on Very Long Instruction Word technology is making this a reality.
  botton Fact File
  botton Brain Teaser
  botton Show Time


Editorials Notes Head

"In the land of the blind, the one-eyed man is king", according to a 2000-year old Greek proverb. Perhaps, but the two-eyed man will always have the competitive edge. Clarity of vision has always been a vital ingredient for success in the semiconductor industry but never more so than now, when SoC (System-on-Chip) technology is redefining the boundaries between market segments and between chip manufacturers and their customers.

As this is the first issue of Challenge in the third millennium, it is hardly surprising that the theme of vision runs through it but there is nothing contrived about this - every article in this issue is included because it is current and reflects where ST is now or where it is heading. Ever since its formation in 1987, ST has grown faster than the world market and increased both its position in the world rankings and its stature within the electronics community. A key factor in this success has been its track record in anticipating its customers' requirements and ensuring that it has the technologies, the products and the infrastructures to meet future needs.

This is particularly borne out by our interview with Dick Pieranunzi who heads up ST's Americas region. The semiconductor industry was born in the USA; any chip manufacturer that wants to succeed at the world level must succeed in America and 1999 was a very successful year for ST in the USA. Not only in terms of sales but also in the ground-breaking developments that took place there, including the customizable VLIW platform developed with Hewlett-Packard (page 7) and the SH-5 processor core developed with Hitachi.

And, talking of vision, it is a year since ST acquired Vision Group, the CMOS imaging specialists. Vision's team of world-class imaging experts has been fully integrated into ST's Imaging and Displays Division and the resulting synergy is enabling the development of many exciting new products, as our lead article illustrates.


Should you require more information, please select the appropriate contact from the "Related Topics" menu.