Section
Author's Guide | Reviewer's Guide

ST Journal of Research
MEMS

Vol. 3, No. 1, August 2006- Art. 6
 
Control of a Z-Axis MEMS Vibrational Gyroscope

MEMS Gyroscope and diagram by
Roberto Oboe, Member, IEEE, Riccardo Antonello, Student Member, IEEE, Ernesto Lasalandra, Guido Spinola Durante, and Luciano Prandi, STMicroelectronics

Copyright
Copyright © IEEE, 2005. Reprinted, with permission, from Control of a Z-Axis MEMS Vibrational Gyroscope, by Roberto Oboe, Riccardo Antonello, Ernesto Lasalandra, Guido Spinola Durante, and Luciano Prandi, IEEE/ASME TRANSACTIONS ON MECHATRONICS, VOL. 10, NO. 4, AUGUST 2005, pagg. 364-370 - doi 10.1109/TMECH.2005.852437
 

Abstract
The paper describes the design of the control loops in a z-axis MEMS vibrational gyroscope operating in a vacuum enclosure. In this device, a silicon mass is driven through an electrostatic actuator so that it has a sinusoidal linear motion with a controlled speed. The design of a suitable controller capable of maintaining the required speed and with prescribed restoring capabilities after shocks is briefly described in the paper. Attached to the driving mass, a second mass, free to move in the direction orthogonal to the motion of the first mass, is subjected to a Coriolis force proportional to the product
of the first mass speed by z-axis rotational speed. The sensing of the Coriolis force and, in turn, of the z-axis rotational speed, is performed in closed loop fashion, with a 1-bit quantized actuation. The restoring force that brings the motion of the second mass to zero is equivalent to the output bit stream of a band-pass sigma-delta converter and contains the information of the Coriolis force. The design of this second control loop and a detailed analysis on the signal-to-noise ratio achievable.

 

Download Art 6 (PDF Format) Size KB 700 page 53