Section
Author's Guide | Reviewer's Guide

ST Journal of Research
Wireless Sensor Networks

Vol. 4, No. 1, May 2007- Introduction
 
Introduction to volume 4, issue 1, of the ST Journal of Research
 
image: wireless sensor networks Ambient Intelligence is a vision where environment becomes smart, friendly, context-aware and responsive to any type of human needs. In this world, computing and networking technology coexist with people in a ubiquitous and pervasive way. In this world, numerous miniature and interconnected smart devices create a new intelligence and interact with each other seamlessly.

Wireless Sensor Networks (WSNs) are one of the first real world examples enabling that vision of Ambient Intelligence. Within a WSN, sensory data originate from multiple sensors of different types spread over potentially wide areas. Virtually any kind of physical quantities such as temperature, voltage, pressure, acceleration, ultrasound, gas flow, etc. can be acquired.
 

Likewise, actuators can be used as a means to influence or control the environment. For coordination and information exchanges, the various nodes communicate over a wireless mesh network in a self-organized manner. Originally motivated by military applications such as battlefield surveillance, the applications of WSNs are many and varied. Industrial and home automation benefit from the capability to wirelessly monitor data that would be difficult or too expensive to monitor using wired sensors. Likewise, health care or environmental control applications take advantage of the miniaturization and self-organized nature of WSNs.

The many potential applications recently motivated major players of the semiconductor industry to invest in this promising field. STMicroelectronics has been among the first companies to enter the WSN market with the introduction of sensors, low-power microcontrollers, wireless radio devices, etc., in its portfolio. STMicroelectronics is a promoter of the ZigbeeTM alliance, an industry consortium working on the definition of network, security and application layers towards truly interoperable WSNs.

One major technical challenge of WSNs is to produce low-cost, low-power and tiny sensor and actuator nodes. Research work is thus needed and involves numerous fields such as Radio Frequency communication, ad-hoc networks, low-power microcontrollers, transduction principles, energy management, middleware, etc. Another key aspect is the coexistence and interoperability of WSNs with existing technologies such as the Internet, broadband wireless networks or database management systems. Given this wide list of topics, this issue of the ST Journal of Research includes several overview papers that help the reader capture the most important challenges as well as a selection of contributions covering specific design topics. Eleven papers have been selected from worldwide recognized experts and ST researchers in the field.

The first section of this special issue includes three tutorial papers. A general introduction to the problems and challenges of developing Wireless Sensor Network devices is given, in the first paper by Chalard et al. from STMicroelectronics. A particular emphasis on ad-hoc networking technologies is proposed in the second paper by Blasi et al. from STMicroelectronics and Bononi from Universita di Bologna. Sheets et al. from the Univeristy of California, Berkeley and Cervini from STMicroelectronics describe in the third paper the main technical challenges faced in the PicoRadio Project carried out at the Berkeley Wireless Research Center.

Four contributions describing the application-specific nature of WSN optimization are included in the second part of the issue. An indoor climate monitoring prototype developed by our STMicroelectronics colleagues illustrate the challenges of integrating WSNs with the Internet via gateway and database client-server tools. Thonet and Bruel from Schneider Electric discuss the mass market adoption of ZigbeeTM solutions in the segments of Building Automation, Home control, Automated Meter Reading and Industrial Automation. The third paper, authored by Yao from UCLA and Lorenzelli from STMicroelectronics, introduces different techniques for source and node localization. In the last paper of this section, Farella et al. from University di Bologna and Urbino expose the reader to the application of WSN and MEMS sensors in the context of body area networks, more specifically posture and activity recognition.

As mentioned above, a WSN device is a complex integrated system implementing a combination of functions such as communication, security and signal or application processing. The last part of the issue includes four papers dedicated to specific design experiences carried out in those areas. Two papers explore the promising use of low data rate UltraWideBand radio communications in the context of WSN. Specifically, Flury et al. from EPFL analyze the impact of impulsive interference on network throughput and energy consumption. Di Benedetto et al. from University La Sapienza focus their work on medium access control schemes proposed for the IEEE 802.15.4a standard. In the third paper Necchi and Lavagno from Politecnico di Torino together with Pandini and Vanzago from STMicroelectronics present their work in trading off power consumption and die area for the design of an asynchronous 8-bit processor. Finally, in the last paper, performances of two Elliptic Curve Cryptography coprocessors are explored by Bertoni from STMicroelectronics together with Breveglieri and Venturi from Politecnico di Milano.

Wireless Sensor Networks have the potential to open a new era. However, as illustrated by the broad range of topics covered by this special issue, technical issues still exist in the production of low-cost small devices operating for years in a self-organized way and seamlessly integrated with Internet access and appropriate human interfaces. We believe that only companies having the capability to master this broad spectrum of activities and to succeed in both “more Moore” and “more-than-Moore” directions will provide winning solutions for Ambient Intelligence.

The Guest Editors would like to thank all the Authors as well as all those involved in the review and editorial process, with a special mention to Antoine Hue for his huge contribution.

 

Julien Zory & Laura Vanzago
Guest Editors