Section
Author's Guide | Reviewer's Guide

ST Journal of Research
Wireless Sensor Networks

Vol. 4, No. 1, May 2007- Art. 9
 
The Aloha access (UWB)2 protocol revisited for IEEE 802.15.4a

image: measurements of delay and throughput in UWB by
Maria-Gabriella Di Benedetto, Luca De Nardis, Guerino Giancola, Daniele Domenicali, School of Engineering, University of Rome La Sapienza

Copyright
Copyright © Università degli Studi di Roma - La Sapienza, 2007
 
Abstract
The IEEE 802.15.4a Task Group recently proposed Impulse Radio Ultra Wide Band (IR-UWB) for a physical layer that can provide combined communication and ranging in low data rate indoor/outdoor networks. At present, it is therefore particularly relevant to design IEEE 802.15.4a MAC strategies that are appropriately tailored on the physical layer. Previously, we proposed the Uncoordinated Baseborn Wireless medium access control for UWB networks (UWB)2, a UWB-tailored MAC based on the low probability of pulse collision. The (UWB)2 adopted the Aloha principle and enabled location-based network optimization by providing and storing estimates of distance between nodes.
This paper first revisits the (UWB)2 MAC protocol in view of its application to IEEE 802.15.4a. The structure of both control and data MAC protocol data units is defined based on the legacy 802.15.4 MAC in order to allow a seamless support, for both centralized and distributed network topologies, as defined in the parent standard. Secondly, this work extends and completes the analysis of (UWB)2 since it takes into account multipath-prone channels. Channel parameters, for both indoor and outdoor propagation scenarios in Line Of Sight (LOS) and Non-Line Of Sight (NLOS) conditions, were derived from the channel model defined within the 802.15.4a channel sub-committee.
Results highlight that the (UWB)2 protocol is robust to multipath, and provides high throughput and low delay, with performance scaling gracefully as a function of the number of users and the user bit rate. Results confirm and support the adoption of (UWB)2 principles for low data rate UWB communications.
 

Download Art 9 (PDF Format) Size 840 KB page 131