Section
 

STMicroelectronics Presents Prototype Silicon Lab-on-chip for DNA Amplification and Detection at Chips-to-Hits

New device builds on company's experience in fluidic MEMS to create compact, inexpensive and rapid solution for point-of-care diagnostics

 Silicon Lab-on-chip forPhiladelphia, October 31, 2002 - At the Chips-to-Hits conference in Philadelphia today, STMicroelectronics (NYSE:STM), the world's third largest semiconductor maker, presented a prototype silicon chip for DNA analysis that integrates both DNA amplification and detection on the same chip. This device is based on Micro-Electro-Mechanical-System (MEMS) technology that applies silicon-chip manufacturing technologies to produce miniature devices with a combination of mechanical, electrical, fluidic and optical elements.

The primary end use targeted by the DNA analysis chip is in medical diagnostics, to detect genetically related disease directly at the point of care without the delays of laboratory testing. Other applications of the DNA analysis chip include drug discovery - the search for more effective new drugs, the testing of livestock for genetic disease, and the monitoring of water supplies for biological contamination.

"The advantage of using silicon rather than plastic or glass for this function is that it has excellent thermal properties, which is extremely useful in analysis techniques like the Polymerase Chain Reaction (PCR) which are based on temperature cycling," said Benedetto Vigna, Manager of ST's MEMS Development Unit. "In addition it can be 'micromachined' readily using well-known and cost effective silicon-chip manufacturing techniques."

Compared to traditional tests, the ST silicon MEMS device offers a very compact solution that reduces the overall testing cost and delivers results in minutes. Using this technology, extremely small quantities of fluid can be analyzed; the limitation is in the external hardware used to transfer samples.

One of the world's leading manufacturers of conventional electronic silicon chips, ST also develops and manufactures silicon MEMS devices using in-house-developed technologies covering a broad range of applications. The microfluidic technology used in the DNA analysis device builds on the company's long experience in the manufacture of inkjet printer chips combining electronic and fluidic elements.

"Our goal in presenting this device to the life sciences community here at Chips-to-Hits," said Barbara Grieco, Business Development Manager in ST's Printhead and Microfluidics Business Unit, "is to identify potential partners in the biomedical field for the joint development of new devices that combine ST's knowhow in silicon MEMS technology with the partners expertise in biomedical technologies and markets." ST currently partners with leading companies in other fields for the joint development of MEMS-based devices for inkjet printers and optical switches.

The prototype DNA analysis device presented at Chips-To-Hits performs DNA amplification in microscopic channels buried in the silicon and then identifies DNA fragments in the sample. DNA amplification is performed using the Polymerase Chain Reaction technique. A prepared DNA sample mixed with suitable reagents flows into the buried channels in the chip where it is repeatedly cycled through three temperatures which doubles the quantity of DNA with each cycle. When the sample has been amplified sufficiently, it flows into a detection area on the same chip where gold electrodes are pre-loaded with DNA fragments. Fragments in the sample attach to matching fragments on the electrodes and are detected optically.

Visit STMicroelectronics at the Chips to Hits Exhibition, 28-30 October, 2002, booth #419,

For more information: www.st.com/mems and http://www.chipstohits.com

About STMicroelectronics
STMicroelectronics, the world's third largest semiconductor company, is a global leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivalled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio and strategic partners positions the Company at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence markets. The Company's shares are traded on the New York Stock Exchange, on Euronext Paris and on the Milan Stock Exchange. In 2001, the Company's net revenues were $6.36 billion and net earnings were $257.1 million. Further information on ST can be found at http://www.st.com.


Should you require more information, please select the appropriate contact from the "Related Topics" menu.