Section
 

High Current, Low Voltage Drop IGBTs from STMicroelectronics

Low power dissipation eases system design

STGE200NB60S Geneva, March 21, 2003 - STMicroelectronics (NYSE: STM) has introduced a 200A version of its advanced family of IGBTs that features low forward-voltage drops at high currents. Such devices belong to the low drop family of ST's IGBTs that ensure low on-voltage losses without using any heavy metal doping or electronic radiation to reduce the life time of minority carries. The parts are designed for use in aluminium welding and induction heating equipment, as well as in UPS and SMPS.

The STGE200NB60S is part of ST's PowerMESH IGBT family, which uses a patented strip layout. The " Mesh overlay" technology is a new strip-based high voltage process made up of a P type mesh structure diffused onto the N-epitaxial layer of an IGBT. The N+ strip that replaces the cells and represents the emitter of the device is then directly diffused onto the P-Mesh layer. The S suffix indicates that this N-channel part has been optimized for low on-voltage drops at operating frequencies of up to 10kHz.

At 600V and 100A, VCE(sat) is less than 1V, at an operating temperature of 100°C. At 200A and an operating temperature of 25°C, VCE(sat) remains below 1.3V .

The efficiency of the part's design means power dissipation in conduction is low. The parts are offered in an insulated ISOTOP package that contributes to safety.

Further information on ST's STGE200NB60S device is available at http://www.st.com/igbt.

About STMicroelectronics
STMicroelectronics is a global leader in developing and delivering semiconductor solutions across the spectrum of microelectronic applications. An unrivalled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio and strategic partners positions the Company at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence markets. The Company's shares are traded on the New York Stock Exchange, on Euronext Paris and on the Milan Stock Exchange. In 2002, the Company's net revenues were $6.32 billion and net earnings were $429.4 million. Further information on ST can be found at http://www.st.com.


Should you require more information, please select the appropriate contact from the "Related Topics" menu.