Section
 

Voltage Reference from STMicroelectronics Saves Power

Small package saves space

TS432Geneva, December 5, 2003 - STMicroelectronics (NYSE: STM) has introduced a low-power, adjustable shunt voltage reference.

The part is designed for use in applications such as power supplies and battery chargers, portable equipment, computers, instrumentation and power management systems.

The TS432 is a low-power shunt voltage reference with a 1.24V output. The output can be adjusted up to 10V using an external resistor bridge. The operating current can be as low as 60µA at 25°C and ranges up to 12mA.

The part is accurate to ±1%, or to ±0.5% for the TS432A variant. Its temperature coefficient is 100 ppm/°C. The parts are typically stable with any capacitive load, and across the industrial temperature range of -40 to +85°C. This eases design.

The part is offered in a space-saving SOT23-3L package.

Further information on these products is available at www.st.com/stdlinear

About STMicroelectronics
STMicroelectronics is a global leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivalled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio and strategic partners positions the Company at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence markets. The Company's shares are traded on the New York Stock Exchange, on Euronext Paris and on the Milan Stock Exchange. In 2002, the Company's net revenues were $6.32 billion and net earnings were $429.4 million. Further information on ST can be found at http://www.st.com.


Should you require more information, please select the appropriate contact from the "Related Topics" menu.