Section
 

Analog Switches from STMicroelectronics Shrink to Fit Smart Mobile Phones and Consumer Applications

Very low on-resistance reduces audio and video distortion

STG3699Geneva, October 17, 2003 - STMicroelectronics (NYSE: STM) has introduced a pair of SPDT analog switches whose packaging and low insertion losses make them ideal for use in consumer products including audio and video devices, cellphones, notebook PCs, PDA and many forms of portable instrumentation.

The STG3699 is a quad SPDT analog switch and the STG3684 is a dual SPDT analog switch. They include multiple "Single Pole Dual Trough" cells and can work in bi-directional mode, using 1.8V compatible digital control pins. The switches are housed in a QFN package that is just 3 x 3mm, making them useful where space is at a premium.

The on-resistance of the devices is less than 0.5Ohm. This reduces distortion to a minimum in audio circuits, ensuring high-fidelity signal routing for products such as cellular phones. The low on-resistance of the parts also means low insertion losses in video applications. Switching times are less than 300ps.

The on-resistance of the switches is matched to within 0.06Ohm, which is useful when switching differential signals.

The parts operate at supply voltages of between 1.65V and 3.6V and are designed to support high current up to ±500mA 10% duty cycle. Power consumption is less than 200nA, making the parts suitable for use in battery-powered systems.

All inputs and outputs are protected against static discharge and transient excess voltages.

Further information on these products is available at www.st.com/stdlogic

STG36xx ARTICLE STG36xx ADVERT

About STMicroelectronics
STMicroelectronics is a global leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivalled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio and strategic partners positions the Company at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence markets. The Company's shares are traded on the New York Stock Exchange, on Euronext Paris and on the Milan Stock Exchange. In 2002, the Company's net revenues were $6.32 billion and net earnings were $429.4 million. Further information on ST can be found at http://www.st.com.

Should you require more information, please select the appropriate contact from the "Related Topics" menu.