Company
ST Home | Analog and Mixed Signal | Real-Time Clocks | M41T6x Ultra-Low Current Family of Serial Real-Time Clocks

Serial Real-Time Clocks
M41T6x Ultra-Low Current Family of Serial Real-Time Clocks

M41T6x Ultra-Low Current Family of Real-Time Clocks (RTCs)Many applications require the date and time, and Real-Time Clocks provide those functions. For example, in data storage applications, all files have date and time attributes that are updated every time a file is created or modified, and the RTC data must be accessed every time that occurs.

RTCs can be implemented in software and in ASIC logic. But maintaining the clock can present added power management challenges. While low-power microcontrollers and ASICs are available, they still draw much more current than a dedicated RTC, and often cannot operate over a wide voltage range.
A better solution is ST’s new M41T6x family of Serial RTCs. These devices lead the way with low current and low voltage operation and come in a tiny QFN package.
M41T6X Family Features
350nA Standby (typ) at 3.0V;
1.3V to 3.6V Operation - timekeeping down to 1.0V;
400KHz I2C Interface;
BCD registers for year, month, day, date, hours, minutes, seconds, 10ths of seconds, and 100ths of seconds;
2 Century bits (Y2.1K compliant);
Automatic Leap Year adjustment;
Lead-free QFN16 package;
–40° to +85°C operating range;
Programmable Alarm and Interrupt;
Programmable Squarewave Output; and
Dedicated 32KHz Output.
Ultra Low Standby Current

The M41T6x family boasts typical standby currents of only 350nA at 3.0V, which makes ST a leader in the marketplace.

These RTCs do not include battery switchover circuits, but are targeted at applications where they are not needed. In many of today’s applications, the entire system is often backed up, so individual components such as the RTCs do not need backup circuitry on chip. Capacitor backup is another example where switchover is not required. The capacitor’s charging diode inherently provides the switchover mechanism.

Handheld applications are a case where the RTC may run off the system battery and also be backed up by a capacitor. And since there is no backup circuitry, the RTC can be made smaller and less costly, and use even lower power. Since current draw is very important in handheld and battery operated systems, the RTC's standby current is a critical parameter. It determines the rate of battery consumption - how long the battery will last - as well as the backup life when using capacitor backup. Drawing only 350nA, users can get from minutes to months of backup time with a capacitor. And they will not encounter the regulatory issues often associated with batteries.

Small QFN16 Package
M41T6x QFN16, 3mm x 3mm PackageToday’s handheld devices put more functions into small packages than ever before, and when users are doing that, they want the smallest packages available. ST’s QFN16 measures only 3mm by 3mm, and is as small as any RTC in the industry.
Low Voltage Operation

While 5V applications are still around, there is shrinking demand for them, but there is growing demand for 3V and 3.3V solutions. Furthermore, the next sweetspot is expected to be 1.8V. Operating from 1.3V to 3.6V, the M41T6x family meets today’s demands, and will meet tomorrow’s, too. Plus, they will keep time all the way down to 1.0V. These are outstanding numbers that should please any user.

In capacitor-backed applications (because they keep time all the way down to 1.0V), the M41T6x series RTCs are able to use more of the charge stored in the backup capacitor, thereby extending the backup life even further. This means less capacitance is required for a given backup time. For the double layer capacitors (“SuperCaps”) often used in these applications, reducing the capacitance lowers the cost.

Lower timekeeping voltage also means that in applications where the system voltage often sags - such as in battery operated and handheld devices - the timekeeping function is made more robust because the voltage must drop to a lower level before the clock begins to lose time. At the end of the day when a handheld unit’s rechargeable batteries have begun to sag, the clock will still be running, and the user will not need to reprogram it.

Oscillator Fail Detect

Brown-out occurs when Vcc drops too low for reliable operation of the circuit, but not low enough to ensure a proper power down/power up sequence. Some registers may get corrupted thereby losing track of the real time.

To detect this brown-out condition, the M41T6x parts include an Oscillator Fail Detect circuit. If, due to low Vcc, the oscillator begins to run intermittently, or stops altogether, a special filter detects this and sets a bit which indicates this event has occurred. The system software now has a bit it can check to confirm whether the time is still good or has possibly been corrupted. This is a key feature for many users, and a major selling point for these devices.

Oscillator Fail Detect Circuit Diagram
Oscillator Fail Detect Circuit


32KHz Output
The M41T62 includes a Watchdog and Alarm, along with a Programmable Squarewave which defaults to 32KHz at power-up. The Calibration feature allows users to get accuracies down to +/–5 seconds per month, and the Oscillator Fail Detect circuit indicates when the time may be corrupted (due to brown-out). 10ths and 100ths of seconds are available for extra fine resolution. Drawing only 350nA at 3.0V, the M41T62 is hard to beat.
M41T6x Block Diagram
M41T62 Block Diagram

 

M41T6x Product Selector
Serial RTC Product Selector
Part Number Data
sheet (PDF)
Product
Page (HTM)
Alarm IRQ Watchdog
Output
Squarewave
Output
32KHz Oscillator Fail Detect
M41T65 M41T65 Datasheet (PDF) ' Alarm IRQ Feature Watchdog Output Feature '' ' Oscillator Fail Detect Feature
M41T62 M41T62 Datasheet (PDF) M41T62 Product Page (HTM) Alarm IRQ Feature Watchdog Output Feature Squarewave Output Feature 32KHz Feature Oscillator Fail Detect Feature
M41T60 M41T60 Datasheet (PDF) M41T60 Product Page (HTM) ' ' ' ' Oscillator Fail Detect Feature
'
More Information
Serial RTC Lead-free Packages Program