Company
ST Home | Diodes | Ultrafast Rectifiers | STTHxxx series extension


STTHxxx series extension
Complete ST bipolar and ultrafast diodes portfolio renewal

ST has been renewing its power rectifiers product range to enlarge the designer choice and improve the power density of each device. After the power Schottky range extension to 170V and the avalanche concept introduction, the next step concerns the reshaping of the bipolar and ultrafast diode portfolio.
 
Introduction to bipolar and ultrafast diodes
Bipolar and ultrafast diodes are the workhorse of all power applications, from PFC converters to PDP and heavy welding converters. The performance of each bipolar or ultrafast diode has a strong impact on the final application performance. However, one critical parameter in an application may be of secondary importance in the other. Most of these functions can be optimized by using ultrafast diodes with medium recovery time value, that is to say not exceeding 75ns, and with maximized performance. Using a new planar platinum doping process instead of the previous gold doping technology, the new STTHxx devices offer optimum solutions in terms of combined low forward voltage drop (VF), low leakage current (IR) and higher operating junction temperatures (up to 175°C).
 
Platinum doping versus gold
The lower the VF, the higher the reverse recovery time trr, this rule is true for both platinum and gold doping ultrafast diodes. Therefore, at a given trr for a diode, the VF can be slightly improved, to the detriment of the leakage current.

By using the planar platinum doping process, ST has reduced the leakage current by approximately 10 to 100 times in comparison with gold doping. Considering the standard reverse recovery time found on the market with the gold doping technology, ST has optimized the VF, trr and IR combined performance of its new devices, now offering the best VF / IR ratio on the market.

Furthermore, the tiny leakage current obtained by this advanced process results in a significant improvement in thermal dissipation, and also contributes to the reduction of the power consumption of the clamping functions in standby mode operation, as well as in low load conditions..
 
STTHxxx series roadmap
The new STTHxxx devices are already available from 200 to 1200V. These new devices replace the STTAxx, BYTxx, BYWxx, BYVxx and STPRxx series.
 
New range features, benefits and availability
The main advantages of the STTHxxx series are:
high operating temperature of 175°C
leakage current divided by 10 to 100 times
low thermal runaway risk thanks to very reduced IR
best VF / IR performance
VFP (forward recovery voltage) specified in datasheets
ultrafast recovery diodes: trr < 80ns (Unitrode conditions)
numerous parametric trade-offs to fit each application
PSPICE parameter available
More packages proposals (DPAK, D²PAK, Fullpack)
to 2fab
Stthxxx New Range Availability