Q.

What is an NVRAM?

A.

NVRAM stands for "Non-Volatile RAM." Most RAMs are volatile; when power is removed, they lose their contents. ROM technologies such as EPROM, EEPROM and Flash retain their contents when power is removed.
An NVRAM is a battery-backed RAM which uses a small Lithium battery to power a Low-Power SRAM when system power is not available thereby creating non-volatile storage like a ROM, but high-speed writeable unlike a ROM. A special circuit called an "NVRAM Supervisor" controls the application of battery power to the LPSRAM.
The Supervisor may be integral to the LPSRAM as in a monolithic, or it may be a separate IC as in a hybrid.
For a short primer on NVRAM, refer to the Application Note AN1012, "Predicting the Battery Life and Data Retention Period of NVRAMs."

[close window]

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Q.

What is a ZEROPOWER® device?

A.

ZEROPOWER is the trademark name for ST's NVRAMs without clocks.

arrowWhat is a ZEROPOWER®?

[close window]

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Q.

What is a TIMEKEEPER®?

A.

TIMEKEEPER is the trademark name for ST's NVRAMs with on-board "Real-Time Clocks." We also have a line of serial access RTCs with small amounts of NVRAM on board. These are sometimes called "Serial TIMEKEEPERs." Also, refer to the following page:

arrowWhat is a TIMEKEEPER®?

[close window]

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Q.

What is an NVRAM Supervisor?

A.

An NVRAM Supervisor provides a switch between the main power supply (Vcc) and a second source of energy (often a lithium battery) in order to supply enough current to a stand-alone SRAM to generate data retention in the event of a power loss. It is said that an NVRAM supervisor "non-volatizes" a stand-alone SRAM.
This concept allows the user to create a customized NVRAM (see the question, "How do I create a high density, surface-mount (> 1Mbit) NVRAM?").

arrowWhat is an NVRAM Supervisor?

[close window]

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Q.

How do you calculate Battery life?

A.

See AN1012, Predicting the Battery Life and Data Retention Period of NVRAMs. Also, refer to the following pages:

arrowSerial RTC Battery Life Data
arrowZEROPOWER® Battery Life Data
arrowTIMEKEEPER® Battery Life Data
arrowSupervisor Battery Life Data

[close window]

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Q.

Why is the M48T08/ T18 I'm using gaining or losing time?

A.

The /INT pin (pin 1) is an open drain output and must be connected to Vcc through a pull-up resistor, even if the interrupt function is not being used.

[close window]

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Q.

How can I calculate the amount of calibration I need?

A.

See AN934, TIMEKEEPER® Calibration.
Also, check out the Calibration Calculator.

[close window]

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Q.

How do I back up a Serial RTC with a SuperCap?

A.

The ST web site provides all of the information, including schematics and a back-up lifetime calculator to help you determine SuperCap size requirements on our SuperCap Calculator page.

[close window]

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Q.

How do I create a high density, surface-mount (>1Mbit) NVRAM?

A.

For high density, the solution is always a hybrid (multi-chip) solution. In a hybrid DIP package, functionally it operates as if there is only one silicon chip inside, but in fact, if you were to open it up, you could see a small board with several components soldered onto it.
For a surface-mount solution, an NVRAM supervisor and one (or more) SRAM(s) are necessary. ST's broad offering of NVRAM Supervisors allows combinations that create NVRAMs not available in our standard ZEROPOWER® and TIMEKEEPER® portfolio.

arrowST's NVRAM Supervisor Combinations

[close window]

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Q.

Are NVRAM packages Lead free?

A.

As part of ST's ECOPACK® program, all NVRAM and Serial RTC products are switching to Lead-free packages.
For more information on this transition to environmentally friendly components and programs, see our Lead Free/RoHS Program web page.

For more details specific to NVRAM and Serial RTC products:

arrowNVRAM Strategy (100K PDF)
arrowNVRAM Qualification Plan (92K PDF)
arrowNVRAM Ordering Information (100K PDF)

[close window]

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Q.

Are STMicroelectronic's battery-backed devices UL certified?

A.

Yes, all ST parts are UL certified.
Details are available on the NVRAM UL Information web page (this link, along with other useful links, is also located on most pages under "Product Support" on the NVRAM web site).

[close window]

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Q.

What is the difference between devices with part numbers starting with "MK" versus those starting with "M"?

A.

In 1994 a new package (the CAPHAT™) was introduced which replaced the old TOPHAT package. The new package is slightly longer and slightly wider than the old package. Products using this new package had the "M" prefix. The "MK" prefix is relevant now to mostly out-of-production products. All new ST NVRAM products use the "M" prefix.

[close window]

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Q.

What does the prefix "MKI" mean?

A.

The "MKI" prefix was for industrial temperature devices. The current designation scheme has the temperature designation in the suffix (usually number "6").

[close window]

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Q.

Are the ST TIMEKEEPER®s Y2K compliant?

A.

One of the types of NVRAM made by ST is the TIMEKEEPER family. These products incorporate a real time clock/calendar which is battery powered when the external supply is not present.
All of our TIMEKEEPER products are Year 2000 compliant. Those which do store the year as only two digits are guaranteed to roll-over correctly from 99 to 00. However, the system software must take into account that these products store only the last two digits of the year. The code should be checked to make sure that the system cannot confuse the indication 00 for the year 1900 instead of the year 2000.
Newer TIMEKEEPER products are designed with a four digit reference for the year and roll-over correctly from 1999 to 2000. Application Note "AN923" explains in detail the solutions to be implemented to avoid Y2K problems in application systems.

[close window]