Main
Features of HD1xxxx Series |
|
Wide range of optimum drive
conditions; Less sensitivity
to the variation of the operating temperature;
Improved R.B.S.O.A for safer switching performance;
Reduced saturation voltage at high current;
High performance 1700V products.
Horizontal deflection requires an application specific characterization
to describe the input requirements needed to minimize the power
losses. The following graph shows the power losses versus the
variation of the base current (IBon) at a fixed output current
of 12A and a switching frequency of 32kHz; these conditions represent
the worst case conditions in wide screen 100Hz TVs. A comparison
with the most advanced device from competition shows the better
performance of HD1750FX (about 1W less).
Power losses curves comparison
| A
Cooler More Reliable System |
The HD1750FX requires a lower base current thus reducing the power
dissipation in the passive components used in the deflection block,
this makes the system a lot cooler and more reliable. It is worth
noticing also that the HD1750FX can operate with a larger IBon
range to ensure the best driving conditions, minimizing as
a result the normal hfe variation with temperature. The
figure below shows the switching waveforms during an application
test performed on a commercial wide real-flat screen TV working
at a switching frequency of 32kHz.

Application oriented switching waveforms
The HD1750FX shows satisfactory performance also at 100kHz confirming
its suitability also in high-resolution 19” monitors as shown
in the losses behaviour graph. This curve is for the ISOWATT218FX
package while even better performance can be achieved with the same
device housed in TO-264.

HD1750FX power losses behaviour
| Part
Numbering Description |
Since the new series has been developed specifically for horizontal
deflection, the part numbers follow the scheme below.
Beside the features that characterize this technology the HDxxxx
series also exhibits a larger RBSOA, offering additional security
during turn-off, where the device could be overstressed by the high
fly-back voltage and the high current which are both present in
anomalous conditions.
Safe operationg area of HD1520FX
|