After receiving many requests from the market, especially from
Japanese TV manufacturers, such as Sharp, Toshiba and Sony, the
new TO-220FH (Fully plastic High voltage) innovative package has
recently been added to the already broad power Bipolar transistor
package portfolio. This package is an upgrade of the popular TO-220FP
package. The creepage path is what makes this package unique from
TO-220FP.
Humidity and foreign material covering the package could affect
the superficial resistivity between leads and between the leads
and the heatsink; however, by increasing the creepage distance
any possible superficial leakage increase is cut. The creepage
distance path between each lead and between the leads and the
heatsink has been increased to >4.0mm, making this package
met all stringent safety norms in high voltage applications. As
well as the advantages that the increase of the creepage path
gives us, this package also offers a competitive low price solution
for the TV market. This package has been tailored to contribute
in making ST a leading supplier in horizontal deflection transistors
for low-end TVs. All devices found in this package can easily
be recognized by the FH suffix in the sales type.
Samples are now available and datasheets can be found on the ST
web. |