Company
ST Home | Transistors | Power MOSFETs | Related Information | STripFET III Technology

STripFET III Technology
Low Voltage Single Feature Size “NH” MOSFETs

The overall success in the low voltage MOSFET market depends primarily on how closely semiconductor suppliers match the expectations of the electronic industry. The improvement in low voltage MOSFET technology continues at a rapid pace as devices with new geometries or greater densities continue to be introduced.

 
The advantages which come from the built-up cell density and scaled-down features are traceable in the lowest on-resistance in the market.
MOSFET - STripFET III Technology

STripFET III Features

ST has just developed a new generation of the well known STripFET technology: STripFET III. This process is also known as EHD3 (Extremely High Density) resulting from the enhanced density of the equivalent cells, well above 57 Mcells/inch².

EHD3’s main feature is the strip width and the inter-strip gaps, which bring a considerable channel perimeter density: W=62m/cm²

High cell density and channel perimeter
Extremely low figure of merit
Optimized intrinsic recovery

EHD Evolution
EHD Evolution table


Figure of merit
Specific RDS(on)
Figure of merit
Specific RDS(on)


MOSFETs - STripFET III
From "NF" to "NH" STripFET

MOSFET STripFET III Relative Efficency at 500kHz
MOSFET STripFET III Buck Converter
Relative Efficiency at 500kHz
Single Phase VIN=12V VOUT=2V
Buck Converter

MOSFET STripFET III Evaluation circuit for efficiency
Evaluation Circuit for Efficiency

STripFET III Features

The main electrical characteristics such as the current capability and RDS(on) are strictly dependent on the channel perimeter per unit area.

Very low RDS(on) gives low conduction losses
Cost effectiveness
Excellent switching behaviour
Reduced power losses of the diode.
MOSFET STripFET III Normalized figure of merit at 4.5V through the EHD generations
Normalized figure of merit at 4.5V through the EHD generations

The EHD3, thanks to the decreased strip width, gains 38% in the channel perimeter per unit area, with respect to the second generation, this also means a great benefit in terms of RDS(on)
The figure of merit (RDS(on) *Qg) has been slashed by 43%. The following graph explains the trend in this parameter, which is of paramount importance in many applications.
On account of the main power supply requirement to operate at the highest efficiency, special attention has been given to the reverse recovery characteristic of the parasitic body diode.
In particular the Qrr is 39% smaller than in the previous EHD generations. Moreover, the low intrinsic resistance, Rg (<1.9ohm) is of outstanding importance to reduce the gate driving power losses. All these improvements are useful attributes in applications, especially for synchronous rectification for motherboard market, that allow us to consider the EHD3 technology as a benchmark in the low voltage scenario.

Applications


Bondless SO-8 Frame
Synchronous buck converter for computer and telecom applications.

Product Range

The effective improvement in the technology has been combined with new packages and new bonding techniques. The bondless SO-8 and PowerSO-8 are the most attractive solutions with a standard pin-out configuration of SO-8. The new ClipPAK has the same clip concept already adopted in the SO-8 package, but without any external difference from a standard DPAK. EHD3 in PowerFLAT and in PowerSO-8 with clip mounting will be available shortly.

MOSFET - STripFET III
Vertical sections of two EHD generations, showing the decreased strip width and a consequent strip density increase of nearly 40% in the third generation