Company
ST Home | Transistors | Power MOSFETs | Related Information | MOSFETs & IGBTs

MOSFETs & IGBTs
High voltage devices for welding

ST covers a consistent part of the rapidly growing welding market in Europe and Asia, while it is the largest supplier in the USA.
MOSFETs and IGBTs are present in both the power factor corrector and inverter stages of welding equipment. A wide range of devices have already been developed for PFCs and a power range will soon become complete for the inverter stage. Focus will be put on devices with fast-recovery body-drain diodes in the 800V and 900V range.

 
The devices already in production are realized with the standard PowerMESH and the first generation MDmesh technology. For products under development, however we are using the latest SuperMESH generation of our standard technology and for advanced devices the improved version of MDmesh. Many of these devices are housed in the ISOTOP package as it is well suited to most welding applications. Its high current and insulation capabilities improve thermal performance and allow safety operations.

Low and High Frequencies

Welding applications can basically be split into low and high frequencies.
The first employs a low frequency transformer (50 to 60Hz) as highlighted in the following block diagrams.

MOSFETS & IGBTs Low frequency welding topologies
Different topologies for low frequency welding

High frequency applications are becoming the most popular, used especially in new designs and based on the configuration shown below.

MOSFETS & IGBTs typical full bridge topology for high frequency welding
Typical full bridge topology for industrial and commercial high frequency welding

Conventional power sources use transformers with the view “the bigger, the better”.
Now, instead, this approach is moving towards the concept of “the smaller, the better”. In fact for a given power, the volume of a transformer is related to the frequency, i.e. increase the frequency and the volume of the transformer will be reduced.

MOSFETS & IGBTs traditional design with low frequency transformer
The higher the switching frequency the lower the size and weight of the welding machine

The result of such an approach is that size and weight are reduced to a minimum i.e. moving from 50Hz to 100kHz the weight is reduced from 70kg to only 3kg. Most welder producers are moving towards this high frequency topology for new designs.



High Frequency Welding Machines

MOSFETs & IGBTs High voltage devices for welding

There are basically two topologies on the primary side, depending on the input voltage: hard-switched asymmetrical half bridge (or 2 transistor forward) for 230V AC and full bridge phase-shift for 400V DC input.In the former case (normally for low power), 500V MOSFETs are used, whereas in the latter 800V or 900V MOSFETs (or 1200V IGBTs) with a fast body diode are needed. As the asymmetrical half bridge can evolve to full bridge, the 500V MOSFETs will also need fast intrinsic diodes. The secondary side employs rectifiers even if AC switches on the same side are used to generate an alternating current with a very high amplitude (~300A) as in the case of welding Aluminium;

in fact the oxide formed during this process can be broken only with an alternating current. Regarding the switch for the inverter stage, we offer a wide range of products depending on the frequency at which the switch has to work.

MOSFETs & IGBTs High frequency solutions in the future
The trend for welding designs is towards high frequency solutions

MOSFETs & IGBTs ST's broad portfolio
ST has a broad portfolio that allows the choice of the right device for all working frequencies