About ST
Products
Applications
Support
Buy
News & Events
ST Worldwide
Contact Us
Login
Application Notes
|
Industrial
|
Motor Control
|
8-bit Microcontrollers
|
ST7 - 8-bit Microcontrollers
PWM management for 3-phase BLDC motor drives using the ST7MC
Application Note
Format:
(1034 kb)
or
(54 kb)
Last Updated: 17/07/2007
Pages: 39
Related Data Briefs
Low voltage motor control demonstration kit based on the ST7MC2S4 and STS8DNH3LL
Related Datasheets
8-bit MCU with nested interrupts, Flash, 10-bit ADC, brushless motor control, five timers, SPI, LINSCI"
Raw Ascii Text
- (
Hide
)
(Unformatted textual content of the document used by search engines)
AN2009 APPLICATION NOTE
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
INTRODUCTION
The ST7MC microcontroller family is the second generation of the 8-bit microcontroller family dedicated to the driving of 3-phase brushless motors. Permanent Magnet Brushless DC motors are replacing DC brush motors more and more in many applications due to advantages such as higher efficiency, quieter operation and better reliability. These motors require the control of an inverter stage. In most cases the switching devices are MOSFET transistors or IGBTs and are organized in a three-phase bridge with free-wheeling diodes as shown in Figure 1. There are two methods of controlling the motor and reading information back from the rotor. These are called the sensor and the sensorless methods. The sensor method uses Hall sensors whereas the sensorless method reads the Back Electromotive Force (BEMF) signal back to determine the position of the rotor and so is less expensive. The ST7MC microcontroller features a dedicated peripheral to drive this type of motor with the best efficiency in order to maintain the advantages of these types of motor. Besides the high flexibility of this dedicated peripheral, its high hardware integration allows cost savings for the application by reducing external components. It is suitable for both sensor and sensorless methods of PM BLDC motor control. Although using the sensorless mode has big advantages in terms of cost and size, it makes the motor drive a little more complicated. The purpose of this application note is to explain in which cases the ST7MC motor control unit can directly read the BEMF voltage and how to quickly set up its control registers in order to use all the advanced features of this product. We will detail and explain the PWM management inside the ST7MC in order to help the developer use all the advantages of this flexibility to optimize the design and the efficiency of the application.
AN2009
Rev 2
1/39
1
Table of Contents
INTRODUCTION . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 1 1 MOTOR CONTROL MACROCELL INTRODUCTION . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3 2 SIX-STEP, 120 DRIVE AND PWM POWER CONTROL . . . . . . . . . . . . . . . . . . . . . . . . . . 5 3 SENSORLESS CONTROL METHODS . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 7 3.1 CLASSIC METHOD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 7 3.2 ST METHOD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 9 4 PWM MANAGER IN VOLTAGE MODE AND CURRENT MODE . . . . . . . . . . . . . . . . . . 10 4.1 PWM MANAGER IN VOLTAGE MODE . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 12
4.1.1 Description . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .12 4.1.2 PWM signal register setting in Voltage mode . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .13
4.2 PWM MANAGER IN CURRENT MODE CONTROL . . . . . . . . . . . . . . . . . . . . . . . . 14
4.2.1 Description . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .14 4.2.2 PWM signal register setting in Current mode . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .16
4.3 SUMMARY VOLTAGE/CURRENT MODE . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 18 5 MANAGEMENT OF PWM AND READING OF BEMF . . . . . . . . . . . . . . . . . . . . . . . . . . . 19 5.1 PWM ON THE HIGH SIDE . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 19 5.2 PWM ON THE LOW SIDE . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 21 5.3 EXAMPLE OF CONFIGURATION OF THE ST7MC REGISTERS . . . . . . . . . . . . . 22 6 SYNCHRONOUS RECTIFICATION . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 25 6.1 SYNCHRONOUS RECTIFICATION PRINCIPLE . . . . . . . . . . . . . . . . . . . . . . . . . . . 25 6.2 SYNCHRONOUS RECTIFICATION CONFIGURATION . . . . . . . . . . . . . . . . . . . . . 27 7 WINDING DEMAGNETIZATION . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 29 7.1 ACCELERATION OF DEMAGNETIZATION WHEN PWM IS APPLIED ON THE LOW SIDE SWITCH 29 7.2 ACCELERATION OF DEMAGNETIZATION WHEN PWM IS APPLIED ON THE HIGH SIDE SWITCH 31 7.3 REGISTERS CONFIGURATION TO ACCELERATE THE DEMAGNETIZATION. . 34 8 CONFIGURATION EXAMPLE . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 35 9 CONCLUSION . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .3. . . . . . 37 9 10 REVISION HISTORY . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 38
2/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
Figure 1. ST7FMC Microcontroller with a three-phase bridge
HV
T0
D0 T2
D2 T4
D4
B
M A
C
T3
D3 T5
D5 T1
D1
Feedback
5V Level shifter Low Side outputs High Side outputs Rotor position inputs ST7FMC
1 MOTOR CONTROL MACROCELL INTRODUCTION
Figure 2 below gives a detailed view of the motor control macrocell included in the ST7MC microcontroller. In bold are the parts of the macrocell that are going to be described in this application note and that have a role in the PWM management. The purpose of this document is to ease the understanding of the PWM management with the ST7MC to control a brushless 3phase DC motor and to make this explanation easier, the schematic on the figure below can be taken as a reference of a global view of the mechanism. Besides the drawings of the functionalities, the names of the registers involved and often even the bits are written in this schematic. Anyhow, each time a register is discussed in this document, either a reference or an exact description will be made for that register.
3/39
1
2
R+ MCPWMU 1 /20 MCPWMV MCPWMW SR bit OSn bits MREF Reg HV
12-bit PWM generator
+1
Compare U
M TI M = FFh?
1 1/128 3 MCO0 MCO2 Dead Time
1/2
ST3-0 bits
4
1 / 2Ratio
-1
SA3-0 & OT1-0 bits SWA bit Z clr
0 1
MZREG < 55h? Ch0 V I
RCH
ck
MTIM [8-bit Up Counter]
8 Ch1
x6
MPWME Reg
Ch3 Ch2
Ch4
High Frequency Chopper
MZPRV Reg [Zn-1] Compare Dead Time SDMn bit DS,H DS 6 Ch5 SZn bit
Compare
R
MPHSTn Reg
ZS,H
drivers
SQ
Dead Time
ZS
DWF[3:0] Filter / C
A x B / 256
ZWF[3:0] Filter / D
MOE bit
MCOMP Reg [Cn+1] CL R-/+ E ZS,H DS,H CS,H
MPAR Reg
MDTG register PCN bit =0
OAON
MPOL Reg
CLI bit
+ CLI
CLIM bit
Compare
OCV bit
CFF[2:0] bit
MISR Reg
CFW[2:0] bit
MIMR Reg
4/39
Board + Motor DS,H CS,H D/Z Window filter
2
Microcontroller ISn bit MCIA MCIB
ZH
Z event generation
+
MCIC
QD
1
MCVREF CS,H VREF DS,H VR2-0
DH CP SPLG
D event generation
XT16:XT8 bit
F mtc
1/4
F periph
V I
PRESCALER
x6
MCO4 B
ZH DH MDREG Reg [Dn]
MZREG Reg [Zn]
A MCO1 MCO3 MCO5 C
Figure 2. Detailed view of the MTC for PM BLDC motor control
DCB bit
n-1 n
MWGHT Reg [an+1]
8
8
8 2 6
6
1
NMCES MCPWMU/V/W
SWA bit
8
OAP OAN OAZ(MCCFI1)
CS,H
A
+ CFAV bit MCCFI0
VDD (I) (V)
MCCREF Cext
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
R1ext
R2ext
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
2 SIX-STEP, 120 DRIVE AND PWM POWER CONTROL
To control a BLDC motor with the best efficiency, we have to know the rotor position at all times. To achieve this there are two modes. One is called the sensor mode, where the information read back from the motor is the one coming from Hall Effect sensors (1 per phase). The other one is the sensorless mode, where the Back Electromotive Force (BEMF) signal information is the one read back from the motor. The strength of the ST7FMC is that it is compatible with all the modes to control a BLDC motor, whether it is sensorless or not and it is even suitable with different variations within the sensorless or sensor modes which will be detailed later on in this application note. In sensorless mode, in order to be able to read the BEMF information, the phase switching has to include a dead time during which no current flows in one of the motor windings. As shown in Figure 4, in six-step, 120 drive, power is removed from each winding every three steps. During this dead-time phase, it is possible to detect the BEMF zero-crossing event on this non powered winding (see Figure 3 for an example). In order to control the speed, the torque or the power applied to the motor, a PWM signal is usually logically ANDed with the switch control signals. This control is implemented by modifying the duty cycle of this logically ANDed PWM signal. With this method, the BEMF voltage is referred to point M of the motor and not to ground. Because this point is at high voltage, the microcontroller cannot read its value directly. Note: In sensor mode the six-step drive or the sinusoidal drive can be implemented as the feedback signal comes independently from the Hall Effect sensor in the dedicated input of the microcontroller. However, in six-step drive, the method will be exactly the same as the one detailed for the sensorless mode. For the sensor sinusoidal mode, the PWM management is the same as for the AC induction motor drive.
5/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
Figure 3. Reading the BEMF (Step 4)
HV
T0
D0 T 2 B
D2 T 4
D4
Read BEMF on phase C M A
B EM F
C
T3
D3 T 5
D5 T 1
D1
Figure 4. Six-step, 120 drive: control signal on the transistor gate
Step Switch
ON
1
2
3
4
5
6
1
2
3
T0 T1 T2 T3 T4 T5
OFF
ON OFF
ON OFF
ON OFF
ON OFF
ON OFF
Node
HV
A
0 HV
B
0 HV
BEMF Voltage
C
0
Note: voltages are represented without any PWM or demagnetization effect.
6/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
3 SENSORLESS CONTROL METHODS
In order to make the BEMF signal readable by the microcontroller and to detect the zerocrossing voltage of this signal, there are two main methods which we will call the classic method for the first one and the ST method for the second. The ST7FMC microcontroller is suitable for both methods. Each method is declinable in sub-method and the ST7MC allows complete flexibility on which sub-method to use. Please refer to the Application Note AN1946 for a complete view and details on all the methods as this document briefly covers only the 2 main methods. 3.1 CLASSIC METHOD The classic method involves dividing and filtering the signal coming from the non-powered phase to make it readable by the 5V microcontroller as shown in Figure 5. A virtual ground is built and is used as the voltage reference to detect the zero-crossing event of the BEMF signal. With this method, the PWM signal which is logically ANDed with the switch control signal can be applied either on the high or on the low side switches as explained in the next section. The ST7MC is able to detect the BEMF zero-crossing signal during either the PWM signal ON time or OFF time.
7/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
Figure 5. Classic sensorless control method
HV
T0
D0 T2
D2 T4
D4
B
M A
C
T3
D3 T5
D5 T1
D1
5V Level Low Side outputs High Side outputs Rotor position inputs internal Vref ST7FMC Virtual ground
shifter
External Vref
Note: The digital filter of ST7MC allows use of the classical method wiring without an analog filter. In that case we can remove the virtual neutral network and replace this by just a voltage divider on the High VOLTAGE BUS. In this situation, sampling at PWM "OFF" is possible only for PWM applied on the high side switch. Please refer to Application Note AN1946 for more details on this method.
8/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
3.2 ST METHOD With the ST Method, by using the free-wheeling diodes during the OFF time of the PWM signal, the M potential is put to ground and the ST7MC microcontroller samples the BEMF signal voltage during the OFF time of the PWM signal. This involves the fact that the PWM has to be applied on the high side and that an OFF time is needed as explained in the next section of this application note. However, fewer external components are required as it is no longer necessary to divide and filter the signal coming from the non-powered winding. As shown in Figure 6, only 3 external resistors are needed to limit the current input in the microcontroller pins.
Figure 6. ST sensorless control Method
HV
T0
D0 T2
D2 T4
D4
B
M A
C
T3
D3 T5
D5 T1
D1
5V Low Side outputs High Side outputs Rotor position inputs internal ST7FMC Vref External Vref
Level Shifter
9/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
4 PWM MANAGER IN VOLTAGE MODE AND CURRENT MODE
The PWM signal logically ANDed with the switch control signal is used to control the power applied to the motor. It can either control the voltage on the motor with a fixed PWM duty cycle or the current by means of an integrated current control circuitry. When the PWM signal controls the voltage, the motor is driven in voltage mode. When it is controlling the current, the motor is driven in current mode. Voltage mode allows you to control the speed easily by changing the motor reference voltage. It does not give you fine control of the current but you can limit the current and consequently the torque to a maximum value. The voltage control is done by the PWM duty cycle. Current mode allows you to permanently control the torque by changing the motor reference current, because torque is proportional to current. The current in the windings is regulated in real time and there is a true DC current flowing through the DC Bus. Current mode also allows the current for each of the 6 steps to be finely controlled as the current control is done during the PWM cycle. Depending on whether the motor is driven in current or voltage mode, the PWM signal does not have the same origin as shown in Figure 7.
10/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
Figure 7. The PWM manager
M C O5 PHASE M EASUREM ENT WINDOW GENERATOR (I) CURRE NT VOLTAG E (V) (I) (V) MO DE U, V, W Phases CFAV bit OAON bit + M C O4 M C O3 M C O2 M C O1 M C O0
NM CES O AP O AN O A Z(M CCFI1) M CCFI0 VDD MCCREF (V) R1 R2
PWM MANAGER
ADC
Phase U
CH ANNE L MANAGER
12-bit counter 1 (V) PCN bit
C
(I)
12-bit THREE-PHASE PWM GENERATOR
R3
Phase U Phase V Phase W
M C P WM U M C P WM V M C P WM W
The PWM manager manages two different integral parts of the way the ST7MC drives the motor: Current regulation or limitation Generation of the PWM signal applied on the switches The PWM manager has two distinct motor driving modes: voltage mode and current mode. In both cases, the motor control 12-bit timer peripheral has an essential role. In Figure 7, the PWM manager uses the paths indicated by the (I) symbol for current mode and by the (V) symbol for voltage mode.
11/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
4.1 PWM MANAGER IN VOLTAGE MODE 4.1.1 Description Figure 8. Current limitation in voltage mode control
ST7MC PWM U output ST7MC TIMER Microcontroller set R Max current reference I
HV T1 A
t
-+ Vdd Rext Rext T4 Max current reference Motor Voltage step time step time T1-T4 T1-T6 VR02139M t
In voltage mode, the PWM of the 12-bit timer (through the compare U register) gives the voltage which is supplied to the motor, it is the voltage control of the motor. This PWM signal is the one logically ANDed with the control switches signal in order to be able to detect the zero-crossing and demagnetization events. In voltage control mode, we can set a limitation to the current. The current limitation can be set by the user with an external resistor divider as shown in Figure 7 (R1 and R2) and Figure 8 (Rext). Usually this current limitation is the one given by the motor manufacturer. When the current feedback reaches the maximum reference current at the comparator input, the transistor to which the PWM is applied is put in off state until the current feedback becomes less than the maximum current limit. So, one of the inputs of the internal comparator is the maximum current limitation, the other input is the current feedback from the motor (MCCFI0 pin or the output of the internal operational amplifier if used as shown in Figure 7). This current limitation is for protection and should normally never be reached when running the motor correctly. Figure 9 is a capture made with an oscilloscope of the different signals in Voltage mode: We can see that the current feedback from the motor never reaches the current limitation and the increase and decrease of the current in the motor corresponds to the PWM signal on the waveform 2.
12/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
Figure 9. Oscilloscope waveforms: Voltage Mode
1. Current in Phase A
2. Signal on High Side Switch of Phase A on Triple Half Bridge Configuration 3. Current Limitation
4. Current Feedback Note: In speed regulation, the PWM duty cycle value only needs to be correct when starting the motor. Once the target speed is reached, the PWM duty cycle will be adjusted automatically by the ST7MC. 4.1.2 PWM signal register setting in Voltage mode In voltage mode, the 12-bit timer is used to set the PWM signal. Compare 0 registers: The compare 0 high and low registers are for setting the frequency of the PWM. COMPARE 0 PRELOAD REGISTER HIGH (MCP0H) Read/Write (except bits 7:4) Reset Value: 0000 1111 (0Fh)
7 0 CP0H 3 CP0H 2 CP0H 1 CP0H 0
Bits 7:4 = Reserved. Bits 3:0 = CP0H[3:0] Most Significant Bits of Compare 0 preload value. COMPARE 0 PRELOAD REGISTER LOW (MCP0L) Read/Write Reset Value: 1111 1111 (FFh)
7 0
CP0L7 CP0L6 CP0L5 CP0L4 CP0L3 CP0L2 CP0L1 CP0L0
Bits 7:0 = CP0L[7:0] Low byte of Compare 0 preload value.
13/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
Compare U registers: The compare U high and low registers are for setting the duty cycle of the PWM signal in voltage mode. COMPARE PHASE U PRELOAD REGISTER HIGH (MCPUH) Read/Write Reset Value: 0000 0000 (00h)
7 0
CPU H7 CPU H6 CPU H5 CPU H4 CPU H3 CPU H2 CPU H1 CPU H0
Bits 7:0 = CPUH[7:0] Most Significant Byte of phase U preload value COMPARE PHASE U PRELOAD REGISTER LOW (MCPUL) Read/Write Read/Write (except bits 2:0) Reset Value: 0000 0000 (00h)
7 CPU L7 CPU L6 CPU L5 CPU L4 CPU L3 0 -
Bits 7:5 = CPUL[7:3] Low bits of phase U preload value. Bits 2:0 = Reserved. 4.2 PWM MANAGER IN CURRENT MODE CONTROL 4.2.1 Description Figure 10. Current regulation in current mode control
ST7MC Microcontroller clock set R TIMER -+ HV T1 A current reference I clock t t
Motor Voltage T4 step time step time T1-T4 T1-T6 VR02139N t
12-bit internal timer PWM output
14/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
In current mode, the PWM output by the 12-bit timer (either MCPWMU, V or W) represents the reference current to be applied to the motor. The PWM duty cycle is the current level at which we want to polarise the motor. At 100% duty cycle, the signal output is at 5V, this corresponds to the maximum current to be applied to the motor for maximum torque. The PWM duty cycle is obtained by dividing the reference current we want in the motor (depending on the torque needed) by the maximum current. For example, if the maximum current is 1A and if the reference current has to be 0.2A, the PWM duty cycle will be 20%. An external resistor and capacitor are added as shown in Figure 7 (R3) and Figure 10 in order to generate the reference current based on a digital to analog converter (DAC) of the PWM signal. So, for the internal comparator, one of the inputs is the current feedback of the motor (MCCFI0 pin or the output of the internal operational amplifier if used), the other input is the reference current given by the filtered PWM signal from the 12-bit timer. We see in Figure 7 and Figure 10 that the internal clock is used in current mode control. The internal clock outputs a PWM signal as well. The frequency of this signal is user-selectable from several values from 390Hz to 50KHz through 4 bits and the off-time of this signal is also user-selectable (from 2.5s to 40s) with a minimum value of 2.5s needed to allow the stabilization of the system if the ST method is used to allow the sampling of the back-EMF signal during off-time. The PWM signal frequency output by the clock represents the current frequency used to supply the motor. The off-time of this PWM signal is variable, with a lower limit of 2.5s in the sensorless mode ST method. The PWM signal output by the internal clock is applied to the designated switch. This mechanism has the following procedure as shown in Figure 10: When the current feedback from the motor reaches the reference current given by the 12-bit timer PWM signal at the comparator input, the internal clock signal is reset. The switch where the PWM is applied is put in an OFF state until the current feedback is lower than the reference current as shown in Figure 10. That's why the duty cycle of the internal clock is variable. A minimum off-time has to be defined by the software programmer in sensorless ST method but the duty cycle is modified depending on the motor behaviour. Figure 11 is a capture done with an oscilloscope of the different signals in Current mode. We can see that as soon as the current back from the motor reaches the level of the current limitation, the PWM signal on waveform 2, meaning the PWM signal on the high side switch of the corresponding phase is put off.
15/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
Figure 11. Oscilloscope waveforms: Current Mode
1. Current in Phase A
2. Signal on High Side Switch of Phase A on Triple Half Bridge Configuration 3. Current Regulation Signal through PWM Compare U filtered 4. Current Feedback Note: In speed regulation, the 12-bit timer PWM duty cycle only has to have the right value to start the motor. Once the target speed is reached, the PWM duty cycle will be adjusted automatically by the ST7MC. 4.2.2 PWM signal register setting in Current mode In current mode, a combination of an internal clock and the output of the current comparator is used to set the PWM signal, the registers described below are the ones used to set the frequency and the minimum OFF time if needed from the PWM signal for the internal clock. PRESCALER & SAMPLING REGISTER (MPRSR) Read/Write Reset Value: 0000 0000 (00h)
7 SA 3 6 SA 2 5 SA 1 4 SA 0 3 X 2 X 1 X 0 X
Bits 7:4 = SA[3:0]: Sampling Ratio. These bits contain the sampling ratio value for current mode. This sets the frequency of the PWM according to the following table
16/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
Table 1. Frequency selection
SA3 0 0 0 0 0 0 0 0 1 1 1 1 1 1 1 1 S A2 0 0 0 0 1 1 1 1 0 0 0 0 1 1 1 1 SA 1 0 0 1 1 0 0 1 1 0 0 1 1 0 0 1 1 SA0 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 Sampling Frequency 50.0 KHz 40.0 KHz 33.33 KHz 25.0 KHz 20.0 KHz 18.1 KHz 15.4 KHz 12.5 KHz 10 KHz 6.25 KHz 3.13 KHz 1.56 KHz 1.25 KHz 961 Hz 625 Hz 390 Hz
PWM REGISTER (MPWME) Read/Write Reset Value: 0000 0000 (00h)
7 X 6 5 4 3 O T3 2 O T2 1 O T1 0 O T0
PW MW PW MV PW MU
The current reference is provided to the comparator by Phase U, V or W of the PWM Generator (up to 12-bit accuracy) and the signal from the three compare registers U, V or W can be output by setting the PWMU, PWMV or PWMW bits. Bits 3:0 = OT[3:0]: Off Time selection These bits are used to select the OFF time in sensorless current mode as shown in the following table
17/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
Table 2. off time table
OT3 0 0 0 0 0 0 0 0 1 1 1 1 1 1 1 1 OT2 0 0 0 0 1 1 1 1 0 0 0 0 1 1 1 1 OT1 0 0 1 1 0 0 1 1 0 0 1 1 0 0 1 1 OT0 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 Off Time sensorless mode (SR=0) (DS[3:0]=0) 2.5 s 5 s 7.5 s 10 s 12.5 s 15 s 17.5 s 20 s 22.5 s 25 s 27.5 s 30 s 32.5 s 35 s 37.5 s 40 s Sensor Mode (SR=1) or sampling during ON time in sensorless (SPLG =1 and/or DS[3:0] bits)
No minimum off time
4.3 SUMMARY VOLTAGE/CURRENT MODE In voltage mode, the 12-bit timer PWM signal (compare U register) gives the voltage to be applied to the motor. This PWM signal is applied to the switches. The internal clock is not used in this mode. A current limitation is implemented in voltage mode. The current limitation can be set by an external divider resistor or by an other PWM signal filtered. In current mode, the 12-bit timer PWM signal gives the reference current to be applied to the motor. This signal has to be filtered by an external RC. The internal clock is used and the PWM signal from the internal clock is applied to the switches. In current mode, the current is regulated by comparing the reference current and the feedback current from the motor.
18/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
5 MANAGEMENT OF PWM AND READING OF BEMF
Depending on the control method used to drive the motor, the PWM signal to detect the BEMF zero voltage crossing signal can be applied in 2 ways: On the high side: During the step, the PWM is applied only on the high side switch, the low side is ON during the complete step. On the low side: During the step, the PWM is applied only on the low side switch, the high side is ON during the complete step. In the ST7MC device, OE [5:0] bits in the MPAR register are used to define whether the corresponding outputs are in high or low side switch position. Then OO [5:0] bits in MPHST register define if the channel is active or not and finally OS [2:0] bits in MCRB register distribute the PWM on the active channels high or low side. Please refer to the product datasheet for the motor control device in the channel manager section for more details or to Section 6 to see a complete configuration. Figure 12. Current during PWM ON time
HV
T0
D0 T 2 B
D2 T 4
D4
M C A HV 2
T3
D3 T 5
D5 T 1
D1
The 2 switches T2 and T3 are ON
5.1 PWM ON THE HIGH SIDE When the related switches are ON, the current passes through the two switches and two motor windings (these are switches T2 and T3 in the example in Figure 12). The potential at point M is HV/2. If nothing is done, the BEMF can not be read by the ST7MC because the voltage is too high to be read by the microcontroller. Using the classic method, the BEMF is divided and filtered as is the rebuilt virtual ground and so the BEMF zero-crossing event can be read when the PWM is ON on the high side switch.
19/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
When the PWM signal is ON when using the Classic method, the voltage at the virtual ground will be HV/2 divided and filtered and the voltage at point C will be (HV/2 + BEMF) divided and filtered so the comparison can be done by the comparator in the microcontroller as it will stay within the microcontroller supply voltage range (0 - Vdd) after division and filtering. When the high side switch PWM is OFF, the current inside the motor continues to flow in the same direction (Figure 13). While the switch is off, the current can only use the diode (D5 in our example). In this case the potential in A is the Von of the T3 switch, the potential in B is -Vf of D5 and the potential at M is (Von-Vf)/2. It is close to zero because in most cases Von = Vf. In this case the microcontroller can read the complete BEMF voltage referred to the ground terminal on the phase C. This is the configuration used for the ST method where the sampling of the BEMF signal is only done during the Off time of the PWM signal. No dividers nor filters are needed externally as we are looking at a signal that is close to the MCU ground level. Note: This sampling method of the BEMF signal is also appropriate for the classic method. In fact the sampling of the BEMF can be done either during ON or OFF time of the PWM for the classic method. Figure 13. PWM on high side: Current during OFF time
HV
T0
D0 T 2 PWM B
D2 T 4
D4
M C A 0V
T3
D3 T 5
D5 T 1
D1
PWM on T2
Free-wheeling diode: D5
current during OFF TIME
20/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
5.2 PWM ON THE LOW SIDE When the related switches are ON (example of Figure 12) the current passes through the two switches and two motor windings. When the low side is switched OFF, the current inside the motor continues to flow in the same direction (Figure 14). While the switch is OFF, the current can only use the diode (D0 in our exam ple). In this case the potential at A is (HV+Vf), the potential at B is (HV-Von) and the potential at M is (2xHV+Von-Vf)/2. We can consider it to be HV (because in most cases Von = Vf). In this case the microcontroller can read the BEMF voltage only if the Classic method is used during ON time of the PWM signal because the signal in C is divided and filtered before the microcontroller input pin. Considering the ST method, the sampling of the BEMF is done only during the OFF time of the PWM and as with the ST method, the signal is not divided and filtered in C before the microcontroller pin, this method can not be used as the voltage in C is close to HV during the PWM off time. Von is the voltage of the switch when it is turned ON Vf is the forward voltage of a diode Figure 14. PWM on low side: Current during OFF time
HV
T0
D0 T 2 B
D 2 T4
D4
M C A HV
T3 PW M
D3 T 5
D5 T 1
D1
PWM on T3; Free-wheeling diode D0
21/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
5.3 EXAMPLE OF CONFIGURATION OF THE ST7MC REGISTERS As explained in section 2 "Sensorless control methods", we have described 2 main sensorless control methods which the ST7MC is compatible with. Please refer to AN1946 for more details. The steps to correctly configure the ST7MC registers depending on the sensorless control method used are as follows: Generate a Pulse Width Modulation signal. If the ST sensorless control method is used, then a 2.5s minimum off time is needed to read the BEMF voltage during the off time (useless in Classic method detection). In Voltage mode (the VOC1 bit is reset in the MCRA register), when driving a PM BLDC motor (the PCN bit is reset in the MDTG register) in six-step drive, a single PWM signal is used to supply the input stage. This PWM signal which is applied to the switches is generated using the 12-bit PWM counter for frequency and the 13 bit compare U register for duty cycle (MCPUL:MCPUH registers). In Current mode (VOC1 bit is set in the MCRA register), the PWM output signal is generated by a combination of the output of the measurement window generator and the output of the current comparator and is directed to the output channel manager as well. This can be done by setting the PWM frequency through SA[3:0] bits in the MPRSR register and the minimum off time using the OT[3:0] bits in the MPWME register. The off time is also dependent on the output of the current comparator as explained in Section 4 of this document. Apply this PWM on the high side or low side switches depending on the sensorless control method used. To do so, you have to configure the microcontroller with the right configuration. In order to configure correctly the registers, this sequence has to be followed. Split the switches in two parts by means of the high side/low side configuration. This is done using the OE [5:0] bits in the MPAR register. PARITY REGISTER (MPAR) Read/Write Reset Value: 0000 0000 (00h)
7 X 6 X 5 OE 5 4 OE 4 3 OE 3 2 OE 2 1 OE 1 0 OE 0
Bits 5:0 = OE[5:0]: Output Parity Mode. 0: Output channel is High 1: Output channel Low For example: T1, T3, T5 low side and T0, T2, T4 high side.
22/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
Select the group you want to read the BEMF from by programming the REO bit in the MPOL register. The group the BEMF is read from depends on the sensorless control method used. If the ST method is used, the high side group has to be selected because the PWM has to be applied on the high side as seen in the previous chapter, therefore, the BEMF can be read only from the high side group, REO bit is reset. If the classic method is used, the BEMF can be read either from the high side group or from the low side group, it depends on where the PWM signal will be applied as described below. So in this configuration, the REO bit can be set or reset. Select also the polarity of the output channel through the MPOL register. POLARITY REGISTER (MPOL) Read/Write (some bits write-once) Reset Value: 0011 1111 (3Fh)
7 ZVD 6 REO 5 OP 5 4 OP 4 3 OP 3 2 OP 2 1 OP 1 0 OP 0
Bit 7 = ZVD: Z vs D edge polarity. 0: Zero-crossing and End of Demagnetization have opposite edges 1: Zero-crossing and End of Demagnetization have same edge Bit 6 = REO: Read on High or Low channel bit 0: Read the BEMF signal on High channels 1: Read on Low channels Note: This bit always has to be configured whatever the sampling method. Bits 5:0 = OP[5:0]: Output channel polarity. These bits are used together with the OO[5:0] bits in the MPHST register to control the output channels. 0: Output channel is Active Low 1: Output channel is Active High. Select the PWM direction after Demagnetization (D) event just before the Zero-crossing (Z) event. The demagnetization event and the corresponding PWM configuration will be explained in Section 5. So the PWM direction can be selected using the OS1 bit in MCRB register. The same is true for the group to read the BEMF from, the PWM can be applied differently depending on the sensorless control method used. If the ST method is used, then the PWM signal has to be applied on the high side, which means that the OS1 bit is reset in MCRB register. If the classic sensorless control method is used, then the PWM signal can be applied either on the high side or on the low side. In both cases, the microcontroller is able
23/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
to detect the BEMF. So, in that case OS1 bit can be set or reset. It depends mainly on the application and on the user. MPHST register bits OO[5:0] are used to put the corresponding output channel active or not. This has to be configured each step over the repetition of the six steps. PHASE STATE REGISTER (MPHST) Read/Write Reset Value: 0000 0000 (00h)
7 X 6 X 5 OO5* 4 OO4* 3 OO3* 2 OO2* 1 OO1* 0 OO0*
Bits 5:0 =OO[5:0]*: Channel On/Off bits These bits are used to switch channels on/off at the next commutation 0: Channel Off, the relevant switch is OFF, no PWM possible 1: Channel On the relevant switch is ON, PWM is possible OO[5:0] Bit Meaning
OO[5:0] 0 1 Output Channel State Inactive Active
* = Preload bits, new value taken into account at next C event In addition to the PWM configuration flexibility, the ST7MC microcontroller features a dead time generator embedded in the motor control peripheral. This is used mainly for the generation of the 3 sinewave 120 shifts for the drive of an AC induction 3-phase motor but it can be used to perform "synchronous rectification" as explained in the next chapter when driving a PM BLDC motor.
24/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
6 SYNCHRONOUS RECTIFICATION
6.1 SYNCHRONOUS RECTIFICATION PRINCIPLE Whatever method is used, the classic method or the ST method, as soon as a PWM signal is logically ANDed with the switch control signal, the free wheeling diodes of the triple half bridge configuration are used during the off time off the PWM signal and the current continues to flow in the same direction in the motor. The ST7MC features a dead time generator that allows application of complementary PWM on the switch adjacent to the one where PWM is applied. With this feature, the conduction losses can be reduced. This is called the "synchronous rectification". Precautions must be taken to avoid short circuits in half bridges. This is ensured by driving high and low side switches with complementary signals and by managing the time between the switching-off and the switching-on instants of the adjacent switches. This time is the deadtime and has to be adjusted depending on the devices connected to the PWM outputs and their characteristics (intrinsic delays of level-shifters, delays due to power switches,...). In the ST7MC, the dead time is set on six dedicated bits in a register allowing a range of dead times from 125ns to 16s. When Fmtc is 16MHz. Dead time can be set with steps of 125, 250 or 500ns. As an example on Figure 14, if the dead time generator is activated, then during the off time of the PWM on T3, T0 will be switched-on so the current will flow through the switch and not through the free-wheeling diode D0. Figure 15 shows the relationship between the output signals of the deadtime register on the adjacent switches and its inputs. O n c e activated, the dead time generator generates two output signals on the adjacent switches: A and B. The A output signal is the same as the input phase signal except for the rising edge, which is delayed relative to the input signal rising edge. The B output signal is the opposite of the input phase signal except the rising edge which is delayed relative to the input signal falling edge.
25/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
Figure 15. Dead times waveform
Reference Input signal
5V 0V
Output A
5V Delay 0V 5V
Output B Delay
0V
Figure 16 and Figure 17 show waveforms of the signal on 2 adjacent switches during synchronous rectification. Figure 17 is a zoom of Figure 16 The dead time has been set in this example to 0.75s. Figure 16. Oscilloscope waveform: synchronous rectification 1
1. Current Waveform in Phase A
2. signal on the high side switch of phase A 3. signal on the adjacent switch, the low side switch of phase A when the synchronous rectification is enabled and a dead time is set
26/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
Figure 17. Oscilloscope waveform: synchronous rectification 2
1. Current Waveform in Phase A
2. signal on the high side switch of phase A 3. signal on the adjacent switch, the low side switch of phase A when the synchronous rectification is enabled and a dead time is set 6.2 SYNCHRONOUS RECTIFICATION CONFIGURATION When driving a PM BLDC motor (PCN bit is reset in MDTG register), the PWM applied to the output channel depends if the motor is driven in voltage or current mode but the dead times are applied in the same way regardless of the source of the PWM signal. As soon as the dead time generator is activated (DTE bit is set in MDTG register), a complementary PWM is applied to the adjacent switch. The dead time value is set-up through the bits DTG [5:0] in MDTG register. The range can go from 125ns to 16s with steps of 125ns, 250ns and 500ns when Fmtc is 16MHz. Note: It is also possible to add a chopper on the PWM signal output using bits HFE[1:0] and HFRQ[2:0] in the MREF register. DEAD TIME GENERATOR REGISTER (MDTG) Read/Write (except bits 5:0 write once-only) Reset Value: 1111 1111 (FFh)
7 PCN DTE DTG5 DTG4 DTG3 DTG2 DTG1 0 DTG0
Bit 7 = PCN: Number of PWM Channels. 0: Only PWM U signal is output to the PWM manager for six-step mode motor control (e.g. PM BLDC motors) 1: The three PWM signals U, V and W are output to the channel manager (e.g. for three-phase sinewave generation)
27/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
Bit 6 = DTE*: Dead Time Generator Enable 0: Disable the Dead Time generator 1: Enable the Dead Time generator and apply complementary PWM signal to the adjacent switch Bits 5:0 = DTG[5:0]*: Dead time generator set-up. These bits set-up the deadtime duration and resolution * = write once-only bit if PCN bit is set, read/write if PCN bit is reset. To clear the DTE bit if PCN=1, it is mandatory to clear the PCN bit first.
28/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
7 WINDING DEMAGNETIZATION
When the microcontroller switches from one step to the next, the non-powered winding needs a certain demagnetization time. During this time, the current in the winding continues in the same direction but decreases to zero. It is not possible to see the BEMF voltage as long as this current is still present, because during this time the voltage on the winding is tied to 0V or HV by the free-wheeling diode. Due to the winding self-induction, the demagnetization time decreases if the reverse voltage on the winding increases. We want to decrease the demagnetization time of the winding so that the window to detect the BEMF zero voltage crossing event is wider. So the goal to decrease this time and to accelerate the end of demagnetization event is to apply the maximum reverse voltage on the winding that needs to be demagnetized. To do so, depending on the previous step configuration as we are going to describe in this section, we can apply either the PWM on the low side switch or on the high side switch to accelerate the demagnetization. Let's look at two examples to illustrate the two possible cases: 7.1 ACCELERATION OF DEMAGNETIZATION WHEN PWM IS APPLIED ON THE LOW SIDE SWITCH Figure 18 shows step 4 (switches T2-T3 are ON) with the normal current and the freewheeling current (dotted line) during the PWM OFF time of the high side switch T2. Figure 18. Step 4 (switches T2-T3 are ON)
HV
T0
D0 T 2 B Norm al current
D2 T 4
D4
free-wheeling current for BEMF reading (ST method) M C
A
T3
D3 T 5
D5 T 1
D1
29/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
When switching from step 4 (switches T2-T3 are ON) to step 5 (switches T4-T3 are ON), a free-wheeling, decreasing demagnetization current is still present through the B terminal (dashed line) and an increasing magnetization current appears through the C terminal (dotted line). Figure 19 shows these two currents during the PWM ON time. Figure 19. Step 5 (switches T4-T3 are ON) during the demagnetization PWM ON time
HV
T0
D0 T 2 B
D2 T 4
D4
Normal mode magnetization current C F T3 D3 T 5 D5 T 1 D1
A
M
PWM on T2
free wheeling demagnetization current
This means, during the PWM ON time: The potential of B is zero The potential of M is close to HV/3 Now depending on the switch we are going to apply the PWM signal, the demagnetization time of winding B will be decreased and the end of demagnetization event will be accelerated during this PWM signal OFF time. The numerous dedicated registers in the ST7MC peripheral allow the flexibility to choose where to apply the PWM signal between the different events. The maximum reverse voltage to decrease the demagnetization time is achieved during the OFF time of the PWM signal.
30/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
Figure 20. Acceleration of demagnetization during low side switch PWM OFF time
HV
T0
D0 T 2 B
D 2 T4
D4
M
Normal current C
A
T3 PW M
D3 T 5
D5 T 1
D1
Demagnetization current
In our example, during step 4 (switches T2-T3 are ON), the VMB voltage on the MB winding was positive. At the beginning of step 5 (switches T4-T3 are ON), the voltage on terminal B will be tied to 0V and the shortest demagnetization configuration is the one that provides the highest voltage at point M to apply the maximum reverse voltage and decrease the demagnetization time. It is easy to verify that the highest voltage (2HV/3) is obtained when the PWM is applied only on the low side switch T3. During the OFF time of this PWM signal (configuration shown in Figure 20), the voltage at point M is 2HV/3. Otherwise if the PWM signal is applied on the high side switch T4, then during the OFF time of the PWM signal, the voltage at point M is 0V. So, in this configuration, the PWM signal has to be applied on the low side switch T3 after the commutation event in order to accelerate the demagnetization time during the OFF time of this PWM signal. 7.2 ACCELERATION OF DEMAGNETIZATION WHEN PWM IS APPLIED ON THE HIGH SIDE SWITCH Figure 21 shows step 3 (switches T2-T1 are ON) with the normal current and the freewheeling current (dotted line) during the PWM OFF time of the high side switch T2.
31/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
Figure 21. Step 3 (switches T2-T1 are ON)
HV
T0
D0 T 2 B Norm al current
D2 T 4
D4
free-wheeling current for BEMF reading (ST method) M C
A
T3
D3 T 5
D5 T 1
D1
When switching from step 3 (switches T2-T1 are ON) to step 4 (switches T2-T3 are ON), a free-wheeling, decreasing demagnetization current is still present through the C terminal (dashed line in Figure 22) and an increasing magnetization current appears through the B terminal (dotted line). Figure 22 shows these two currents during the PWM ON time. Figure 22. Step 4 (switches T2-T3 are ON) during the demagnetization PWM ON time
HV
T0
D0 T 2
D2 T 4
D4 free wheeling demagnetization current
Normal mode B magnetization current
A
M
C
T3
D3 T 5
D5 T 1
D1
PWM on T2
This means, during the PWM ON time: The potential of B is HV
32/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
The potential of M is close to 2HV/3 Now depending on the switch we are going to apply the PWM signal ON, the demagnetization time of winding C will be decreased and the end of demagnetization event will be accelerated during this PWM signal OFF time. The goal is to apply the maximum reverse voltage on winding C. Figure 23. Acceleration of demagnetization during high side switch PWM off time
HV
T0
D0 T 2
D2 T 4
D4
Normal mode B magnetization current
demagnetization current
A
M
C
T3
D3 T 5
D5 T 1 Normal current
D1
PWM on T2
In our example, during step 3 (switches T2-T1 are ON), the VMC voltage on the MC winding was negative. At the beginning of step 4 (switches T2-T3 are ON), the voltage on terminal C will be tied to HV and the shortest demagnetization configuration is the one that provides the lowest voltage at point M to apply the maximum reverse voltage and decrease the demagnetization time. It is easy to verify that the lowest voltage HV/3 is obtained when the PWM is applied only on the high side switch T2. During the OFF time of this PWM signal, the voltage at point M is HV/ 3 (configuration shown in Figure 23). Otherwise if the PWM signal is applied on the low side switch T3, then during the OFF time of the PWM, the voltage at point M is HV. So, in this configuration, the PWM signal has to be applied on the high side switch T2 after the commutation event in order to accelerate the demagnetization time.
33/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
7.3 REGISTERS CONFIGURATION TO ACCELERATE THE DEMAGNETIZATION. The ST7MC allows you to program different PWM configurations in sensorless mode. In sensor mode, the demagnetization event is useless as the feedback information is not read from the windings. In order to minimize the demagnetization time in sensorless mode, the ST7MC allows you to modify the PWM direction between the step commutation and the end of demagnetization. In sensorless mode the OS2 bit in register MCRB enables the PWM on the high side or low side channels between the commutation and the demagnetization event. Table 3. OS bits in MCRB register
OS2 bit PWM after C and before D OS1 bit PWM after D and before Z On High Channels 1 0 On High Channels 0 1 On Low Channels 1 0 0 1 On Low Channels 0 1 On Low Channels 1 On High Channels 1 OS0 0 0 PWM after Z and before next C On high channels On low channels On high channels On low channels On high channels On low channels On high channels On low channels
D event: Demagnetization C event: Commutation Z event: BEMF zero voltage crossing event
34/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
8 CONFIGURATION EXAMPLE
This section gives a configuration example for a six-step 120 motor drive for a PM BLDC motor in sensorless, current and autoswitched mode. The sensorless control method used would be the ST method. The configuration registers can be divided in two parts: Table 4 lists the configuration bits that only need to be written once, Table 5 gives the step-dependent configuration bits. The registers in Table 2 must be updated within each commutation interrupt routine in order to select the configuration for the next step. Table 4. General Configuration Registers
Register MPAR MCRA MCRB MCRC MDTG 7 6 5 TES1 TES0 O E 5 0 0 1 MOE CKE SR 1 1 0 Value 4 3 2 1 0 O E 4 O E 3 OE2 O E 1 O E 0 0 1 0 1 0 DAC V0C1 SWA PZ DCB 0 1 1 X X Comments Outputs 0, 2, 4 are HIGH channels Outputs 1, 3, 5 are LOW channels The motor runs in autoswitched mode, current mode, sensorless mode. PWM after end of demagnetization: on HIGH channels.
MPHST
Res CPB HDM SDM OCV OS2 OS1 OS0 0 S S S S S 0 1 OI HZ SZ S C SPLG V R 2 V R 1 V R 0 Hardware Z event Sampling at the end of PWM off time 0 1 0 0 0 X X X PCN DTE DTG5 DTG4 DTG3 DTG2 DTG1 DTG0 Only PWM U is output to the PWM manager 0 0 0 0 0 0 0 0 No Dead time generator IS1 IS0 OO5 OO4 OO3 OO2 OO1 OO0 Input selection and output data change at each step. S S S S S S S S
Notes: - Bits marked with X depend on the motor and / or the application: PZ depends on the noise present in the application, DCB depends on the motor symmetry; VR[2:0] bits depend on the noise level on the BEMF input pins. - Bits marked with S have to be modified after each commutation (step dependent configuration). These bits are summarized in Table 4. Those bits are taken in account only at the next commutation event.
35/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
Table 5. Step Configuration Registers
Step Current direction High side Low side OO<5-0> output bits Measure done on terminal: Connected to pin IS<1:0> selection bits value MPHST Back EMF shape CPB value for BEMF detection (ZVD=0) Voltage on measured point at the start of demagnetization Transition at end of demagnetization Hardware demagnetization HDM-HDM bit value (Hard - Soft Demagnetization Mask bits) 1 A to B T0 T5 100001 C MCIC 10 2 A to C T0 T1 000011 B MCIB 01 3 B to C T2 T1 000110 A MCIA 00 4 B to A T2 T3 001100 C MCIC 10 5 C to A T4 T3 011000 B MCIB 01 6 C to B T4 T5 110000 A MCIA 00
10100001 01000011 0 0 0110 10001100 01011000 00110000 Falling 0 0V 0V->BEMF (r ising) always possible 10 Rising 1 HV Falling 0 0V Rising 1 HV Falling 0 0V Rising 1 HV
HV0V->BEMF HV0V->BEMF HV->BEMF >B EMF >BEMF (r ising) (r ising) (falling) (falling) (falling) not always always not always always not always possible possible possible possible possible 11 10 11 10 11
PWM side selection for acceler- Low Side High Side Low Side High Side Low Side High Side ating demagnetization Driver selection for accelerating T5 T0 T1 T2 T3 T4 demagnetization OS2 bit 0 1 0 1 0 1 MCRB xx010001 xx111101 xx010001 xx111101 xx010001 xx111101
36/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
9 CONCLUSION
As seen in this document, the ST7MC with the features of its dedicated peripheral offers a lot of combinations for the PWM management when driving a BLDC motor. Thanks to a high hardware integration (both digital and analog) and a high flexibility of configuration through dedicated registers, the PWM management can be fine-tuned and optimized to reach and maintain the best efficiency of the motor whatever the control method. This flexibility combined with the fact that the ST7MC family comes with the 8-bit ST7 core, a very well known and stable core, and is offered in a wide range of packages (8Kbytes to 60Kbytes memory size Flash/ROM and from 32 pins to 80 pins) allow this part to be suitable for all the motor control applications requiring a scalar motor control. The associated development kit, ST7MC-KIT/BLDC, that is provided with full C libraries software and reference hardware design allows you to get his application up and running in a minimum amount of time for a better "time to market". In conclusion, a good time to market, high performances and cost savings are the keys of a successful design done with the ST7MC.
37/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
10 REVISION HISTORY
Table 6. Document revision history
Date
06-Jan-2005 12-Jul-2007
Revision
1 2
Changes
Initial release Removed references to obsolete products
38/39
PWM MANAGEMENT FOR 3-PHASE BLDC MOTOR DRIVES USING THE ST7MC
Please Read Carefully: Information in this document is provided solely in connection with ST products. STMicroelectronics NV and its subsidiaries ("ST") reserve the right to make changes, corrections, modifications or improvements, to this document, and the products and services described herein at any time, without notice. All ST products are sold pursuant to ST's terms and conditions of sale. Purchasers are solely responsible for the choice, selection and use of the ST products and services described herein, and ST assumes no liability whatsoever relating to the choice, selection or use of the ST products and services described herein. No license, express or implied, by estoppel or otherwise, to any intellectual property rights is granted under this document. If any part of this document refers to any third party products or services it shall not be deemed a license grant by ST for the use of such third party products or services, or any intellectual property contained therein or considered as a warranty covering the use in any manner whatsoever of such third party products or services or any intellectual property contained therein. UNLESS OTHERWISE SET FORTH IN ST'S TERMS AND CONDITIONS OF SALE ST DISCLAIMS ANY EXPRESS OR IMPLIED WARRANTY WITH RESPECT TO THE USE AND/OR SALE OF ST PRODUCTS INCLUDING WITHOUT LIMITATION IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE (AND THEIR EQUIVALENTS UNDER THE LAWS OF ANY JURISDICTION), OR INFRINGEMENT OF ANY PATENT, COPYRIGHT OR OTHER INTELLECTUAL PROPERTY RIGHT. UNLESS EXPRESSLY APPROVED IN WRITING BY AN AUTHORIZED ST REPRESENTATIVE, ST PRODUCTS ARE NOT RECOMMENDED, AUTHORIZED OR WARRANTED FOR USE IN MILITARY, AIR CRAFT, SPACE, LIFE SAVING, OR LIFE SUSTAINING APPLICATIONS, NOR IN PRODUCTS OR SYSTEMS WHERE FAILURE OR MALFUNCTION MAY RESULT IN PERSONAL INJURY, DEATH, OR SEVERE PROPERTY OR ENVIRONMENTAL DAMAGE. ST PRODUCTS WHICH ARE NOT SPECIFIED AS "AUTOMOTIVE GRADE" MAY ONLY BE USED IN AUTOMOTIVE APPLICATIONS AT USER'S OWN RISK. Resale of ST products with provisions different from the statements and/or technical features set forth in this document shall immediately void any warranty granted by ST for the ST product or service described herein and shall not create or extend in any manner whatsoever, any liability of ST. ST and the ST logo are trademarks or registered trademarks of ST in various countries. Information in this document supersedes and replaces all information previously supplied. The ST logo is a registered trademark of STMicroelectronics. All other names are the property of their respective owners. 2007 STMicroelectronics - All rights reserved STMicroelectronics group of companies Australia - Belgium - Brazil - Canada - China - Czech Republic - Finland - France - Germany - Hong Kong - India - Israel - Italy - Japan Malaysia - Malta - Morocco - Singapore - Spain - Sweden - Switzerland - United Kingdom - United States of America www.st.com
39/39
Document Number: 10691