About ST
Products
Applications
Support
Buy
News & Events
ST Worldwide
Contact Us
Login
User Manuals
|
Microcontrollers
|
8-bit Microcontrollers
|
ST7 - 8-bit Microcontrollers
Front panel based on STFPC320
User Manual
Format:
(1595 kb)
or
(57 kb)
Last Updated: 05/10/2007
Pages: 36
Related Data Briefs
VFD display controller with power management RTC and other front panel control/display functions using the STFPC320
Related Datasheets
8-bit MCU with 16 to 60K Flash/ROM, ADC, CSS, 5 timers, SPI, SCI, I2C interface
Front panel controller/driver with standby power management and real-time clock
Raw Ascii Text
- (
Hide
)
(Unformatted textual content of the document used by search engines)
UM0440 User manual
Front panel based on STFPC320
Introduction
This document explains the functioning of the front panel evaluation board based on the STFPC320 which consists of the front panel controller STFPC320 and microcontroller ST72F325 as I2C master. The basic idea is to develop a front panel for the DVD Recorder which is very close to the available solutions in the market. The objective of this evaluation board is to display the capabilities of ST's front panel controller/driver STFPC320 to fit the market segment of front panel of DVD players, DVD Recorders, VCR, Home Theater with Clock feature, HTiB (Home Theater in a Box), Personal Video Recorders (PVRs), Set-top boxes and other applications that require a compact, integrated solution, keeping the system cost as low as possible. The focus in the design of the system has been in 2 key areas - a Standby management feature for low power consumption and an embedded real time clock in the STFPC320 for auto wake-up and setting the recording start and end time. The system can be operated using:
Front panel keys Remote control
In the sections below the operation of the system is explained. When the board is connected to the power supply, the system is ready to perform any operation. At the time of manufacturing an additional board has been connected to allow in-circuit programming of the microcontroller. The two can be easily separated so that the front panel board can be used independently. To summarize, the key features of the demonstration board are:
16-segment, 11-digit customized VFD for DVD Recorder 14 front panel keys 4 LEDs (Red for standby, Yellow for schedule, Blue for IR and Green for Mute) 1 IR sensor for the remote control operation Buzzer on the board for Mute feature demonstration Real Time Clock to set the timer and alarm for wake-up On-board I2C EEPROM for time logging for automatic operations Power supply connector for four power supplies (3.3 V , 12 V, -30 V and GND) Standby management for low power operation Auto wake-up feature from system standby Embedded in-circuit programming capability
September 2007
Rev 1
1/36
www.st.com
Contents
UM0440
Contents
1 Getting started . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 6
1.1 1.2 1.3 1.4 1.5 System requirements . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 6 Package content . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 6 Hardware installation . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 6 Powering on the system . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 7 Default setting of the system . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 8
2
Using the front panel evaluation board . . . . . . . . . . . . . . . . . . . . . . . . . . 9
2.1 Application keys . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 9
2.1.1 2.1.2 2.1.3 2.1.4 2.1.5 2.1.6 2.1.7 2.1.8 OPEN/CLOSE . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 9 PLAY/PAUSE . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 9 NEXT/FF . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 10 PREV/RR . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 11 RECORD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 11 STOP . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 12 MUTE . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 13 STANDBY . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 13
2.2
Menu keys . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 14
2.2.1 2.2.2 2.2.3 2.2.4 2.2.5 MENU/SET . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 14 UP . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 14 DOWN . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 14 + . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 14 - . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 14
2.3
Hot keys . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 15
2.3.1 2.3.2 2.3.3 OPEN/CLOSE . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 15 PLAY/PAUSE . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 15 PIN_AV8 . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 15
3
Using the MENU options . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 16
3.1 3.2 3.3 3.4 SYS TIME . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 16 ALRM TIME . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 19 START REC . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 21 STOP REC . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 22
2/36
UM0440
Contents
3.5 3.6 3.7 3.8 3.9
MEDIA selection . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 24 ERASE MEDIA . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 25 BRIGHTNES . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 25 VOLUME . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 26 EXIT . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 27
4
Using the remote control . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 28
4.1 4.2 4.3 4.4 4.5 4.6 4.7 POWER . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 28 MUTE . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 29 PLAY/PAUSE . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 29 FORWARD/NEXT . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 29 PREV/RR . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 29 VOLUME + & - . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 29 BRIGHTNESS + & - . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 30
5
Revision history . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 35
3/36
List of figures
UM0440
List of figures
Figure 1. Figure 2. Figure 3. Figure 4. Figure 5. Figure 6. Figure 7. Figure 8. Figure 9. Figure 10. Figure 11. Figure 12. Figure 13. Figure 14. Figure 15. Figure 16. Figure 17. Figure 18. Figure 19. Figure 20. Figure 21. Figure 22. Figure 23. Figure 24. Figure 25. Figure 26. Figure 27. Figure 28. Figure 29. Figure 30. Figure 31. Figure 32. Figure 33. Figure 34. Figure 35. Figure 36. Figure 37. Figure 38. Figure 39. Figure 40. Figure 41. Figure 42. Figure 43. Figure 44. Figure 45. Figure 46. Figure 47. Figure 48. Front panel using STFPC320 - front view. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 6 Front panel using STFPC320 - back view . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 7 Power supply connections . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 7 Power-on condition, HELLO displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 7 System stable, ready to use . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 8 OPEN displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 9 CLOSE displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 9 PLAY displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 9 PAUSE displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 10 FORWARD displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 10 FORWARD in background (RECORDING ongoing). . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 10 FORWARD in background (MENU processing) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 11 REWIND displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 11 REWIND in background (RECORDING ongoing). . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 11 REWIND in background (MENU processing) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 11 RECORDING displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 12 REC END displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 12 Real-time Clock displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 12 MUTE LED (green) is ON . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 13 System in STANDBY - STANDBY followed by RTC displayed on VFD . . . . . . . . . . . . . . . 13 Menu keys . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 14 Hot keys . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 15 MENU displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 16 SYS TIME displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 16 _ displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 16 Setting the value at hh:mm:ss location . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 17 Cursor at hh:mm:ss location . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 17 Cursor at hh:mm:ss location . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 17 Cursor returns to first location. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 18 Using - key to set time . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 18 ALRM TIME displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 19 ERROR displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 19 Alarm set - SCH LED (yellow) ON . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 19 System standby & alarm time set . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 20 ALARM displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 20 START REC displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 21 STOP REC displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 22 REC END displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 23 NO REC displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 23 MEDIA HDD displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 24 MEDIA DVD displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 24 ERASE DVD displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 25 ERASE HDD displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 25 BRIGHTNES displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 25 Brightness level displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 26 Maximum brightness level selected . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 26 VOLUME displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 26 Volume level displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 27
4/36
UM0440 Figure 49. Figure 50. Figure 51. Figure 52. Figure 53. Figure 54.
List of figures Change in volume level . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 27 EXIT displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 27 IR LED blinks . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 28 MUTE OFF displayed on VFD . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 29 Schematic page 1 . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 31 Schematic page 2 . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 32
5/36
Getting started
UM0440
1
1.1
Getting started
System requirements
The system operates in stand-alone mode by powering externally using a power supply (ESICOM Code: STEVAL-ISA029V1) containing four outputs (3.3 V, 12 V, -24 V and GND) with current capacity of 500 mA. For power supply connection refer to Section 1.4.
1.2
Package content
The evaluation board package includes the following:
Hardware One demonstration board One Power supply connector (7-way) User manual
Documentation
1.3
Hardware installation
The evaluation board can be powered through an external power supply having four outputs (3.3 V, 12 V, -24 V and GND) whose ESICOM code is STEVAL-ISA029V1. Figure 1. Front panel using STFPC320 - front view
The major components present on the board - front view are (see Figure 1), 1. 2. 3. 4. 5. 6. 7. 8. 9. External connector for the power supply input 16-segment, 11-digit customized VFD 4 status LEDs - Standby, Schedule, IR and Mute 14 Front panel keys IR sensor VFD controller/driver Microcontroller I2C based EEPROM Voltage Regulator
10. HE10 connector for ICC programming
6/36
UM0440 Figure 2. Front panel using STFPC320 - back view
Getting started
The major components present on the board - back view are (see Figure 2), 1. Buzzer for demonstrating mute feature
1.4
Powering on the system
This is an easy to use system. As soon as the DC power supply (ESICOM Code: STEVALISA029V1) is plugged in, the system is up and running. The power supply connections should be made as shown in Figure 3. Figure 3. Power supply connections
At power on "HELLO" is visible on the VFD (see Figure 4). Figure 4. Power-on condition, HELLO displayed on VFD
7/36
Getting started
UM0440
After some time, approximately 4-5 seconds "NO DISC" is visible on the VFD (see Figure 5), which indicates that the system is stable and ready for use. Figure 5. System stable, ready to use
Note:
As long the system is not stabilized i.e. "HELLO" is displayed, the user should not perform any operation.
1.5
Default setting of the system
The system is programmed with following default settings: 1. 2. 3. Brightness of display is set to the maximum level i.e. 14/16 Volume is set to be the lowest level i.e. only one bar, as shown in Figure 48. The medium selected is DVD.
Note:
Each time the board is powered up, the system time should be set otherwise the behavior of the real time clock is not guaranteed.
8/36
UM0440
Using the front panel evaluation board
2
2.1
Using the front panel evaluation board
Application keys
Application keys are the keys on the front panel evaluation board with which some operations can be performed. There are 8 application keys on the board.
2.1.1
OPEN/CLOSE
The OPEN/CLOSE is a key with toggle functionality. When the key is pressed for the first time after Power On, "OPEN" is visible on the VFD, as shown in Figure 6. Figure 6. OPEN displayed on VFD
On the second key press," CLOSE" is displayed on the VFD, as shown in Figure 7. Figure 7. CLOSE displayed on VFD
On subsequent key press operations, the VFD display toggles between "OPEN" and "CLOSE" depending upon the last message displayed. Note: On pressing the OPEN/CLOSE key, the selected media icon (DVD or HDD) is visible on the left side of the VFD.
2.1.2
PLAY/PAUSE
Like the OPEN/CLOSE key, the PLAY/PAUSE key also has toggle functionality. When the key is pressed for the first time after Power On, "PLAY" is displayed on the VFD along with the play icon ( ) on the left side of the VFD, as shown in Figure 8. Figure 8. PLAY displayed on VFD
9/36
Using the front panel evaluation board
UM0440
On the second key press," PAUSE" is displayed on the VFD along with the pause icon (II) on the left side of the VFD, as shown in Figure 9. Figure 9. PAUSE displayed on VFD
On subsequent key press operations, the VFD display toggles between "PLAY" and "PAUSE" depending upon the last message. Also, if other operations such as recording start either due to RECORD key press or record timer setting or we enter menu mode, the text message changes but the play icon ( ) or the pause icon (II) (depending on the system state) on the left side of the VFD remains on. This changes only if the system enters standby or keys such as OPEN/CLOSE, STOP, NEXT/FF and PREV/RR are pressed.
2.1.3
NEXT/FF
On the NEXT/FF key press, "FORWARD" is displayed on the VFD along with the forward icon ( ) on the left side of the VFD, as shown in Figure 10. This text message "FORWARD" is seen scrolling from left to right. Figure 10. FORWARD displayed on VFD
Subsequently, if other operations such as recording start either due to RECORD key press or record timer setting (see Figure 11) or we enter menu mode (see Figure 12), the text message changes but the forward icon ( ) on the left side of the VFD remains on. The icon changes only if the system enters standby or keys such as OPEN/CLOSE, PLAY/PAUSE, STOP and PREV/RR are pressed. Figure 11. FORWARD in background (RECORDING ongoing)
10/36
UM0440
Using the front panel evaluation board Figure 12. FORWARD in background (MENU processing)
2.1.4
PREV/RR
On the PREV/RR key press, "REWIND" is displayed on the VFD along with the rewind icon ( ) on the left side of the VFD, as shown in Figure 13. This text message "REWIND" is seen scrolling from right to left. Figure 13. REWIND displayed on VFD
Subsequently, if other operations such as recording start either due to RECORD key press or record timer setting (see Figure 14) or we enter menu mode (see Figure 15), the text message changes but the rewind icon ( ) on the left side of the VFD continues to be on. The icon changes only if the system enters standby or keys such as OPEN/CLOSE, PLAY/PAUSE, STOP and NEXT/FF are pressed. Figure 14. REWIND in background (RECORDING ongoing)
Figure 15. REWIND in background (MENU processing)
2.1.5
RECORD
The RECORD key is an indication of the recording feature support offered by the device STFPC320. On the RECORD key press, "RECORDING" is displayed on the VFD along with the record icon (REC) on the left side of the VFD, as shown in Figure 16.
11/36
Using the front panel evaluation board Figure 16. RECORDING displayed on VFD
UM0440
To stop recording, press the RECORD key again. "REC END" is displayed on the VFD glass and record icon is turned off, as shown in Figure 17. Another way to stop recording is by setting the recording end time, using the menu option. This is described in Section 3.4. Figure 17. REC END displayed on VFD
Note:
The recording is stopped if the system goes in Standby mode.
2.1.6
STOP
The STFPC320 device has a built-in real-time clock (RTC). Upon pressing the STOP key, the clock is displayed on the VFD glass in the hh:mm:ss format, as shown in Figure 18. The clock is displayed in 24-hour clock mode. Figure 18. Real-time Clock displayed on VFD
Note:
For details on RTC mode refer to the STFPC320 datasheet.
12/36
UM0440
Using the front panel evaluation board
2.1.7
MUTE
The system's Mute feature can be demonstrated using the MUTE front panel key. If the MUTE LED (green LED) is ON (see Figure 19), this indicates that the system is in mute mode (no sound). On pressing the MUTE key, the Buzzer present on the back side of the board does not buzz. Figure 19. MUTE LED (green) is ON
If the MUTE LED is OFF which means the system is not in mute mode, then on pressing the MUTE key the buzzer buzzes. Note: Note: MUTE can be activated and deactivated using Remote Control Only. The volume of the buzzer is not affected by the volume setting of the system.
2.1.8
STANDBY
On the STANDBY key press, the STDBY LED (red LED) on the front panel board glows indicating system in standby, as shown in Figure 20. All the front panel keys except the hot keys (explained in Section 2.3) are non-functional. The VFD display is on and "STANDBY" is displayed on the VFD. After 4-5 seconds the text disappears and the real-time clock is displayed (see Figure 20). Figure 20. System in STANDBY - STANDBY followed by RTC displayed on VFD
The system wakes up from Standby by using the following options: 1. Hotkey a) b) 2. Note: Using the front panel keys (see Section 2.3) Using the remote control (see Section 4.1 and Section 4.3)
Alarm time setting (Section 3.2, 3.3 and 3.4)
For details on STANDBY mode and management refer to the STFPC320 datasheet.
13/36
Using the front panel evaluation board Note: If keys are pressed simultaneously, the behavior of the system is not guaranteed.
UM0440
2.2
Menu keys
On the right side of the Board (see Figure 21), there are 5 keys which are used for entering into the menu mode and setting the system time, alarm time, media, erasing media, brightness-level and volume control. Figure 21. Menu keys
2.2.1
MENU/SET
The MENU/SET key is used to enter the menu and to confirm the various settings selected.
2.2.2
UP
The UP key is used to navigate through the various menu options.
2.2.3
DOWN
The DOWN key is used to navigate through the various menu options.
2.2.4
+
The '+' key is used to move the cursor on the VFD glass in the right direction. This key is used for time setting options, brightness-level and volume control.
2.2.5
The '-' key is used to move the cursor on the VFD in the left direction. This key is used for time setting options, brightness-level and volume control.
Note: Note:
The UP, DOWN, + and - keys are active as long as the system is in menu mode otherwise, they are non-functional. If keys are pressed simultaneously, the behavior of the system is not guaranteed.
14/36
UM0440
Using the front panel evaluation board
2.3
Hot keys
To wake up the system from standby we can use the HOT keys. When the system is in standby i.e. the STBY LED (red LED) is ON (see Figure 20 ) and any one of the Hot Key is pressed, the system wakes up. The STBY LED turns OFF and the system restarts. "HELLO" is displayed on the VFD (see Figure 4) and the function related to the hot key is performed. The Front panel demo board has three (3) Hot Keys (see Figure 22), as explained below. Figure 22. Hot keys
2.3.1
OPEN/CLOSE
If the system is in standby and OPEN/CLOSE key is pressed, the system wakes up i.e. STBY LED turns OFF and "HELLO" is displayed on the VFD (seeFigure 4). After 4-5 seconds, "OPEN" is displayed on the VFD (see Figure 6).
2.3.2
PLAY/PAUSE
If the system is in standby and PLAY/PAUSE key is pressed, the system wakes up i.e. STBY LED turns OFF and "HELLO" is displayed on VFD (see Figure 4). After 4-5 seconds, "PLAY" is displayed on the VFD (see Figure 8).
2.3.3
PIN_AV8
If the system is in standby and the PIN_AV8 key is pressed, the system wakes up i.e. STBY LED turns OFF and "HELLO" is displayed on VFD (see Figure 4). After 4-5 seconds, "NO DISC" is displayed on the VFD (see Figure 5).
Note: Note:
If the PIN_AV8 key is pressed when the system is not in Standby, then "NO DISC" is displayed on the VFD (see Figure 5). If keys are pressed simultaneously, the behavior of the system is not guaranteed.
15/36
Using the MENU options
UM0440
3
Using the MENU options
On pressing the MENU/SET key, you enter the menu mode. "MENU" is displayed on the VFD (see Figure 23). Various menu options such as setting the system time, alarm time, media, erasing media, brightness-level and volume control are available to perform certain system settings. Figure 23. MENU displayed on VFD
Use the UP and DOWN key to navigate through the various menu options. MENU/SET key is used to select any menu option. + and - keys are used for moving the cursor in right and left directions respectively on the VFD (see Figure 21 for menu keys). After, you exit from the menu mode; "NO DISC" is displayed on the VFD (see Figure 5). There are total of 9 menu options, as explained below.
3.1
SYS TIME
SYS TIME is for setting the system time i.e. initializing the real-time clock. Follow the below mentioned steps to set the system time: 1. 2. Press the MENU/SET key, "MENU" is displayed on the VFD (see Figure 23). Press the DOWN key once, "SYS TIME" is displayed on the VFD (see Figure 24).
Figure 24. SYS TIME displayed on VFD
3.
Press the MENU/SET key again, to select the menu option. "_" (underscore) is displayed on the VFD (see Figure 25) at the hh:mm:ss location.
Figure 25. _ displayed on VFD
16/36
UM0440 Note:
Using the MENU options To set the system time as 00:00:00, press the MENU/SET key again after step 3. "NO DISC" is displayed on the VFD i.e. exit from menu mode. Press the STOP key to verify and immediately the real-time clock is displayed on the VFD . The below mentioned steps explain setting the system time as 15:24:12. 4. To increase and decrease the numeric value use the UP and DOWN key respectively (see Figure 26)
Figure 26. Setting the value at hh:mm:ss location
5.
Move to the next location using the + key (right side). Now the cursor is at hh:mm:ss location (see Figure 27). Repeat steps 4 and 5 until you reach the last location i.e. hh:mm:ss (see Figure 28).
Figure 27. Cursor at hh:mm:ss location
Figure 28. Cursor at hh:mm:ss location
17/36
Using the MENU options
UM0440
6.
The cursor keys are cyclic. When you reach the last location and the + key is pressed again, the cursor moves to the first location (see Figure 29). The data displayed is erased and the new numeric value can be set using the UP and DOWN keys.
Figure 29. Cursor returns to first location
7.
In case you are at the last location and the data at the previous location needs to be changed, use the - key. The cursor move one place in the left direction (see Figure 30). The data is erased and new numeric value can be set using the UP and DOWN keys.
Figure 30. Using - key to set time
8. 9.
If you are ok with the time set, press the MENU/SET key to set the time as system time. "NO DISC" is displayed on the VFD (see Figure 5) and the system exits from menu mode.
10. This can be verified by pressing the STOP key; real-time clock is displayed on the VFD (see Figure 18). Note: Note: The system clock is in 24 hours clock format; make sure to set the time based on that. When the system is powered on, the system time should be set. If System time is not set after every power up, then the clock can show a random value, and consequently the interrupt signals (if set) can occur at wrong times or may not occur. If some previous alarm settings are stored in the system, upon resetting the system time, the alarms are cleared.
Note:
18/36
UM0440
Using the MENU options
3.2
ALRM TIME
ALRM TIME is for scheduling the alarm time. This is used for self-system wake-up if it is in standby mode. Follow the below mentioned steps to set the alarm time: 1. 2. Press the MENU/SET key, "MENU" is displayed on the VFD glass (see Figure 23). Press the DOWN key twice, "ALRM TIME" is displayed on the VFD (see Figure 31).
Figure 31. ALRM TIME displayed on VFD
3. 4. 5.
Press the MENU/SET key again, to select the menu option. "_" (underscore) is displayed on the VFD (see Figure 25) at the hh:mm:ss location. To increase and decrease the numeric value use the UP and DOWN key respectively (see Figure 26). Move to the next location using the + key (right side). Now the cursor is at hh:mm:ss location (see Figure 27). Repeat steps 4 and 5 until you reach the last location i.e. hh:mm:ss (see Figure 28). If the alarm time selected is less than the current system time and MENU/SET key is pressed, "ERROR" is displayed on the VFD (see Figure 32) and the alarm time is not set. The system exits from the menu mode.
6.
Figure 32. ERROR displayed on VFD
7.
If the alarm time selected is greater than the current system time and MENU/SET key is pressed, "NO DISC" is displayed on the VFD (see Figure 5) and the alarm time is set. The system exits from the menu mode. Also, the SCH LED (yellow LED) turns ON, indicating that an alarm sequence has been scheduled for the system (see Figure 33).
Figure 33. Alarm set - SCH LED (yellow) ON
19/36
Using the MENU options
UM0440
We will now consider two cases for alarm time setting and the corresponding system behavior.
Case 1: System in Standby and Alarm time set If the system is in standby mode and alarm time has been set, then both STBY LED (red LED) and SCH LED (yellow LED) are glowing (see Figure 34).
1.
Figure 34. System standby & alarm time set
2. 3.
When the system time matches the alarm time, it is system wake-up condition from standby mode. The STBY LED (red LED) and SCH LED (yellow LED) turn OFF. "HELLO" is displayed on the VFD (See Figure 4). After 4-5 seconds, "ALARM" is displayed on the VFD glass (see Figure 35).
Figure 35. ALARM displayed on VFD
Case 2: System not in Standby and Alarm time set If the system is not in standby mode and alarm time has been set, then SCH LED (yellow LED) turns ON (see Figure 33). When the system time matches the alarm time, it is simply an alarm indication for the system. The SCH LED (yellow LED) turns OFF and "ALARM" is displayed on the VFD glass (see Figure 35).
1. 2. 3. Note: Note: Note:
The alarm time to be set should be greater than the system time, otherwise the error condition is generated and the alarm time is not set. The SCH LED turns OFF if system time matches the alarm time, only if no other alarm sequence has been set such as for recording. The alarm clock is also in 24 hours clock format; make sure to set the time based on that.
20/36
UM0440
Using the MENU options
3.3
START REC
START REC is the time at which the system automatically starts recoding. In case the system is in standby mode, it wakes up from the scheduled recording time and starts recording. Follow the below mentioned steps to set the recording start time: 1. 2. Press the MENU/SET key, "MENU" is displayed on the VFD (see Figure 23). Press the DOWN key three times, "START REC" is displayed on the VFD (see Figure 36).
Figure 36. START REC displayed on VFD
3. 4. 5.
Press the MENU/SET key again, to select the menu option. "_" (underscore) is displayed on the VFD (see Figure 25) at the hh:mm:ss location. To increase and decrease the numeric value use the UP and DOWN key respectively (see Figure 26). Move to the next location using the + key (right side). Now the cursor is at hh:mm:ss location (see Figure 27). Repeat steps 4 and 5 until you reach the last location i.e. hh:mm:ss (see Figure 28). If the record start time selected is less than the current system time and MENU/SET key is pressed, "ERROR" is displayed on the VFD (see Figure 32) and the start record time is not set. The system exits from the menu mode. If the start record time selected is greater than the current system time and MENU/SET key is pressed, "NO DISC" is displayed on the VFD (see Figure 5) and the start record time is set. The system exits from the menu mode. Also, the SCH LED (yellow LED) turns ON, indicating that an alarm sequence has been scheduled for the system (see Figure 33).
6.
7.
We will now consider two cases for start record time setting and the corresponding system behavior.
Case 1: System in Standby and Start Record time set If the system is in standby mode and start record time has been set, then both STBY LED (red LED) and SCH LED (yellow LED) are glowing (see Figure 34). When the system time matches the start record time, it is system wake-up condition from standby mode along with recording to start. The STBY LED (red LED) and SCH LED (yellow LED) turn OFF. "HELLO" is displayed on the VFD (See Figure 4). After 4-5 seconds, "RECORDING" is displayed on the VFD (see Figure 16).
1. 2. 3.
21/36
Using the MENU options
UM0440
Case 2: System not in Standby and Start Record time set If the system is not in standby mode and start record time has been set, then SCH LED (yellow LED) turns ON (seeFigure 33). When the system time matches the start record time, it is simply the start of recording time. The SCH LED (yellow LED) turns OFF and "RECORDING" is displayed on the VFD (see Figure 16).
1. 2. 3. Note: Note: Note:
The start record time to be set should be greater than the system time, otherwise the error condition is generated and the time is not set. The SCH LED turns OFF if system time matches the alarm time, only if no other alarm sequence has been set such as for alarm time. The start record clock is also in 24 hours clock format; make sure to set the time based on that.
3.4
STOP REC
STOP REC is the time at which the system automatically stops recoding. Follow the below mentioned steps to set the recording stop time: 1. 2. Press the MENU/SET key, "MENU" is displayed on the VFD (see Figure 23). Press the DOWN key four times, "STOP REC" is displayed on the VFD (see Figure 37).
Figure 37. STOP REC displayed on VFD
3. 4. 5.
Press the MENU/SET key again, to select the menu option. "_" (underscore) is displayed on the VFD (see Figure 25) at the hh:mm:ss location. To increase and decrease the numeric value use the UP and DOWN key respectively (see Figure 26). Move to the next location using the + key (right side). Now the cursor is at hh:mm:ss location (see Figure 27). Repeat steps 4 and 5 until you reach the last location i.e. hh:mm:ss (see Figure 28). If the record stop time selected is less than the current system time and MENU/SET key is pressed, "ERROR" is displayed on the VFD (seeFigure 32) and the stop record time is not set. The system exits from the menu mode. If the record stop time selected is less than the pre-set record start time and MENU/SET key is pressed, "ERROR" is displayed on the VFD (see Figure 32) and the stop record time is not set. The system exits from the menu mode. If the record stop time set is greater than current system time and/or pre-set record start time and MENU/SET key is pressed, "NO DISC" is displayed on the VFD (see Figure 5) and the stop record time is set. The system exits from the menu mode. Also, the SCH LED (yellow LED) turns ON, indicating that an alarm sequence has been scheduled for the system (see Figure 33).
6.
7.
8.
22/36
UM0440
Using the MENU options We will now consider three cases for stop record time setting and the corresponding system behavior.
Case 1: Recording ongoing and stop record time set If the system is not in standby mode, recording is ongoing and stop record time has been set, then SCH LED (yellow LED) turns ON (see Figure 33). When the system time matches the stop record time, it simply stops recording. The SCH LED (yellow LED) turns OFF and "REC END" is displayed on the VFD (see Figure 38).
1. 2. 3.
Figure 38. REC END displayed on VFD
Case 2: Recording not started and stop record time set If the system is not in stand by mode, recording has not been started and stop record time has been set, then SCH LED (yellow LED) turns ON (see Figure 33). When the system time matches the stop record time, it is an indication of recording failure. The SCH LED (yellow LED) turns OFF and "NO REC" is displayed on the VFD (see Figure 39).
1. 2. 3.
Figure 39. NO REC displayed on VFD
Case 3: System in Standby and stop record time set If the system is in standby mode and stop record time has been set, then both STBY LED (red LED) and SCH LED (yellow LED) turn ON (see Figure 34). When the system time matches the stop record time, it is system wake-up condition from standby mode along with recording failure. The STBY LED (red LED) and SCH LED (yellow LED) turn OFF. "HELLO" is displayed on the VFD (see Figure 4). After 4-5 seconds, "NO REC" is displayed on the VFD (see Figure 39).
1. 2. 3.
Note: Note: Note:
The stop record time to be set should be greater than the system time, otherwise the error condition is generated and the time is not set. The stop record time to be set should be greater than the start record time, otherwise the error condition is generated and the time is not set. The SCH LED turns OFF if system time matches the alarm time, only if no other alarm sequence has been set such as for alarm time.
23/36
Using the MENU options Note:
UM0440
The stop record clock is also in 24 hours clock format; make sure to set the time based on that.
3.5
MEDIA selection
The system has been designed to support two types of media devices - DVD and HDD. Depending upon the media selected the symbol on the left side of the VFD glass glows. Follow the below mentioned steps for media selection: 1. 2. Press the MENU/SET key, "MENU" is displayed on the VFD (see Figure 23). Press the DOWN key five times. If the previously selected media is DVD, then "MEDIA HDD" is displayed (see Figure 40).
Figure 40. MEDIA HDD displayed on VFD
Otherwise, if the previously selected media is HDD then, "MEDIA DVD" is displayed (see Figure 41). Figure 41. MEDIA DVD displayed on VFD
3.
To select the new media device, press MENU/SET key. "NO DISC" is displayed on the VFD (see Figure 5) and the system exits from the menu mode. Also, depending upon the media selected, the symbol on the left side of the VFD glows. DVD for DVD and HDD for HDD.
24/36
UM0440
Using the MENU options
3.6
ERASE MEDIA
The system has been designed to support two types of media devices for erase - DVD and HDD. Depending upon the media selected, the symbol on the left side of the VFD glows. Follow the below mentioned steps for media erase, 1. 2. Press the MENU/SET key, "MENU" is displayed on the VFD (see Figure 23). Press the DOWN key six times. If the selected media is DVD, then "ERASE DVD" is displayed (see Figure 42).
Figure 42. ERASE DVD displayed on VFD
Otherwise, if the selected media is HDD then, "ERASE HDD" is displayed (see Figure 43). Figure 43. ERASE HDD displayed on VFD
3.
To select the media erase option, press MENU/SET key. "NO DISC" is displayed on the VFD (see Figure 5) and the system exits from the menu mode.
3.7
BRIGHTNES
The BRIGHTNES menu option is used to set the brightness level of the VFD display. By default the brightness level set at the maximum level (14/16). This can be changed by using this Menu option. STFPC320 supports 8 levels of brightness - 1/16, 2/16, 4/16, 10/16, 11/16, 12/16, 13/16, and 14/16. Follow the below steps to change the system display brightness: 1. 2. Press the MENU/SET key, "MENU" is displayed on the VFD (see Figure 23). Press the DOWN key seven times, "BRIGHTNES" is displayed on the VFD (see Figure 44).
Figure 44. BRIGHTNES displayed on VFD
25/36
Using the MENU options
UM0440
3.
Press the MENU/SET key once; vertical bars are displayed, indicating the current brightness level (see Figure 45). Both the glow of the vertical bar and the position on the VFD grid indicate the brightness level. The level increases from left to right, and so does the intensity of the glow.
Figure 45. Brightness level displayed on VFD
4.
Use the '+' or '-'keys to increase or decrease the brightness level. Figure 46 shows the maximum brightness level (14/16).
Figure 46. Maximum brightness level selected
5. Note:
To set the selected brightness level, press the MENU/SET key again. "NO DISC" is displayed on the VFD (see Figure 5) and the system exits from the menu mode.
On every power up the system wakes up with the last set level of Brightness, as there is an external EEPROM present on the demo board.
3.8
VOLUME
The VOLUME menu option is used to set the volume level. By default the volume level is set at the minimum level. This can be changed by using this menu option. Follow the below mentioned steps to change the volume, 1. 2. Press the MENU/SET key, "MENU" is displayed on the VFD (see Figure 23). Press the DOWN key eight times, "VOLUME" is displayed on the VFD (see Figure 47).
Figure 47. VOLUME displayed on VFD
26/36
UM0440
Using the MENU options
3.
Press the MENU/SET key once; vertical bars are displayed, indicating the current volume level (see Figure 48).
Figure 48. Volume level displayed on VFD
4.
Use the '+' or '-'keys to increase or decrease the volume level. Figure 49 shows the change in volume level.
Figure 49. Change in volume level
5. Note: Note: Note:
To set the selected volume level, press the MENU/SET key again. "NO DISC" is displayed on the VFD (see Figure 5) and the system exits from the menu mode.
The boards default volume level is set to minimum. On every power the board wakes up with the last set level of Volume, as there is an external EEPROM present on the demo board. The volume control does not affect the volume of the Buzzer sound. This feature is provided just to demonstrate that the volume control can also be adjusted using the STFPC320 switch pins.
3.9
EXIT
1.To come out of the menu mode, the EXIT command is provided. The last option of the menu list is exit. On reaching the last option, using the DOWN key, "EXIT" is displayed on the VFD (see Figure 50). Press the MENU/SET key again. "NO DISC" is displayed on the VFD (seeFigure 5) and the system exits from the menu mode. Figure 50. EXIT displayed on VFD
Note: Note:
The user can leave the menu at any time by pressing any APPLICATION key. When the user is in the EXIT menu, pressing the DOWN key makes nothing happen but pressing the UP key makes the pointer move to the previous menu i.e. VOLUME.
27/36
Using the remote control
UM0440
4
Using the remote control
The system has been designed to work for RC5, TV1 remote control protocol. As the application is being used for the demo purpose only, all the keys of the remote control are not supported. The keys supported in this application are:
Power Mute, Play/ Pause, PREV/ RR (Rewind), Next/ FF (Forward), Volume '+' & '-' Brightness '+' & '-'.
Another feature supported by this system is the IR indicator LED. Each time an IR command is sent from the remote control, the IR LED (blue LED) blinks, indicating IR data transfer (see Figure 51). Figure 51. IR LED blinks
The following features/ commands detailed in the next sections are supported by the remote control.
4.1
POWER
The system is put into Standby using the POWER key. The STBY LED (red LED) turns ON (see Figure 20). To wake up the system from standby the same key can also be used as it is a toggle key. On wake-up "HELLO" is displayed and the STBY LED (red LED) turns OFF (see Figure 4). After 4-5 seconds the system stabilizes and "NO DISC" is displayed (see Figure 5).
28/36
UM0440
Using the remote control
4.2
MUTE
This system feature is only supported through the remote control Mute key. The system is put into MUTE by pressing the "MUTE" key. "MUTE" is displayed on the VFD and the MUTE LED (green LED) turns ON (see Figure 19). As long the system is mute, the buzzer on the back side of the demo board does not buzz (if the MUTE front panel key is pressed). Again, the Mute key of the remote control is a toggle key, and if it is pressed for the second time, the system exits from mute mode. "MUTE OFF" is displayed on the VFD and the MUTE LED (green LED) turns OFF (see Figure 52). Now, if the Mute front panel key is pressed, the buzzer buzzes. Figure 52. MUTE OFF displayed on VFD
Note:
If the system is put into MUTE mode and the volume level is being changed/ set through the menu options using the front panel keys, then the system also remains in MUTE mode. The system can leave mute mode only through the MUTE key of the remote control.
4.3
PLAY/PAUSE
The PLAY Key on the remote control functions the same way as the PLAY/PAUSE key on the front panel. For details refer to Section 2.1.2. See Figure 8 and Figure 9. Similar to the front panel key, PLAY/PAUSE key on remote control also works as a hot key. For details refer to Section 2.3.2. See Figure 4 and Figure 8.
4.4
FORWARD/NEXT
The NEXT/FF Key on the remote control functions the same way as the NEXT/FF key on the front panel. For details refer to Section 2.1.3. See Figure 10.
4.5
PREV/RR
The PREV/RR Key on the remote control functions the same way as the PREV/RR key on the front panel. For details refer to Section 2.1.4. See Figure 13.
4.6
VOLUME + & The Volume key functions the same way as the volume menu option explained in Section 3.8. See Figure 48.
29/36
Abbreviations
UM0440
4.7
BRIGHTNESS + & The Brightness key functions the same way as the brightness menu option explained in Section 3.7. See Figure 45.
Appendix A
Table 1.
No. 1. 2. 3. 4. 5. 6. 7. 8. 9. 10. 11.
Abbreviations
Abbreviations
Acronym RTC I2C EEPROM VFD LED DVD HDD ICC GND IR RC5 Definition Real Time Clock Inter-integrated circuit Electrically Erasable Programmable Read Only Memory Vacuum Fluorescent Display Light Emitting Diode Digital Versatile Disc Hard Disk Drive In-circuit communication Ground Infrared Remote Control Protocol by Philips
30/36
UM0440
Appendix B
5
LED1 LED2 LED4 IRQ_N/SQW PIN_AV8 SCL SDA G(1) G(2) G(3) G(4) G(5) F1
4
3
2
VCC3.3V
52 51 50 49 48 47 46 45 44 43 42 41 40
U2 VFD1 VCC3.3V R11 10K S/KS(1) C5 100nF S/KS(2) S/KS(3) S/KS(4) S/KS(5) S/KS(6) S/KS(7) S/KS(8) S/KS(9) S/KS(10) XIN R10 33K
R3 10R
S2
S3 R16 18K XIN XOUT ST FPC320_T QFP52 S(16)/G(13) S(15)/G(14) S(14)/G(15) S(13)/G(16) KEY1 KEY2
-
MUT E ST BY
R15 18K
LED1 LED2 LED3 LED4 IRQ_N/SQW PIN_AV8 SCL SDA GRID1 GRID2 GRID3 GRID4 GRID5
+
1 2 3 4 5 6 7 8 9 10 11 12 13 SEG1/KS1 SEG2/KS2 SEG3/KS3 SEG4/KS4 SEG5/KS5 SEG6/KS6 SEG7/KS7 SEG8/KS8 SEG9/KS9 SEG10/KS10 SEG11/KS11 SEG12/KS12 VSS OS C SW 1 SW 2 MU T E ST BY VDD XIN XOUT GN D KEY1 KEY2 READY IR-DAT A_IN
G(6) G(7) G(8) S(20)/G(9) S(19)/G(10) S(18)/G(11)
Figure 53. Schematic page 1
C7
100nF
R ESET _ N VDD GRID6 GRID7 GRID8 SEG20/GRID9 SEG19/GRID10 SEG18/GRID11 SEG17/GRID12 SEG16/GRID13 SEG15/GRID14 SEG14/GRID15 SEG13/GRID16
39 38 37 36 35 34 33 32 31 30 29 28 27
READY
14 15 16 17 18 19 20 21 22 23 24 25 26
R5 2.7K VSS-30V C1
S/KS(11) S/KS(12)
R19 100R
1
25pF C3 32.768Khz XOUT 25pF
Y1
2 3
4
S(13)/G(16) S(14)/G(15)
C10 VCC3.3V 10uF/tant
IR1
S/KS(1) S/KS(2) S/KS(3) S/KS(4) S/KS(5) S/KS(6) S/KS(7) S/KS(8) S/KS(9) S/KS(10) S/KS(11) S/KS(12)
10K
R18
S(15)/G(14) S(16)/G(13)
GND VCC3.3V NC OUT IR SENSOR
4 3 2 1
STFPC320 CIRCUIT
VCC3.3V S(18)/G(11) S(19)/G(10)
R27 VDD_MICRO U4 KF40BD
R25
R26
STANDBY CIRCUIT
VCC12V
S(20)/G(9) G(8) G(7)
10K
4K7
4K7
U5 ST 72F325K4T 6_T QFP_32P
IRQ_N/SQW READY
VDD_2 VAREF
2.2uF C17 0.1uF R30 220R ST BY
25 1
C15
SDA SCL
R28 R29
100R 100R
16 17 18 19 VOUT VIN GN D GN D GN D GN D NC INHIBIT 2 1 PD0/AIN0 PD1/AIN1 PE0/T DO PE1/RDI 31 32 26 27
PA3 PA4 PA6/SDAI PA7/SCLI
1 2 3 4
8 7 6 5
C16 0.1uF
G(6) G(5) G(4) G(3) G(2) G(1)
28 29 30
PB0 PB3 PB4
1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31 32 33 34 35 36 37 38 39 40 41 42 43 44 45 46 47 48 49 50 51 52 53 54 55 56
J4 ICC JUMPER R4 10R
Demonstration board schematic
F1 NX NP NP S1 IC S2 S3 IC S4 IC S5 S6 S7 IC S8 S9 S1 0 IC IC S1 1 S1 2 IC S1 3 S1 4 IC IC S1 5 S1 6 NC IC NC NC NC IC NC NC IC NC 1G 2G IC 3G 4G 5G IC 6G 7G 8G 9G 10G 11G NP NP NX F2
ICCDAT A
PF0/MCO/AIN8 PF1/BEEP PF4/OCMP1_A/AIN10 PF6/ICAP1_A PF7/EXT CLK_A R ESET
C18 0.01uF
3 4 5 6 7 21
RESET
FUT ABA-11-MT -141NK
ICCCLK
8 9 10 11 12 13 14 15
PC0/AIN12/OCMP2_B PC1/AIN13/OCMP1_B PC2/ICAP2_B PC3/ICAP1_B PC4/ICCDAT A/MISO PC5/AIN14/MOSI PC6/ICCCLK/SCK PC7/AIN15/SS
C19 OSC1
F2
OSC1 OSC2
24 23
OS C 1 OS C 2
VFD FILAMENT
25pF C20 Y2 16MHz OSC2 25pF T itle
VPP/ICCSEL
20
VPP/ICCSEL
R31 10K
2 22
VSSA VSS_2
MICROCONTROLLER CIRCUIT
Size B Document Number ST Mic
Demonstration board schematic
31/36
U1 74VHC14MT R VCC3.3V 100nF VCC3.3V C11 100nF VCC12V C13 100nF VCC12V + C14 10uF CON7 + C12 10uF RESET VPP/ICCSEL + J3 ICC CONNECT OR
330R
Q3 ST D790AT 4
3
2
VCC3.3V D2 1N5817 D3 1N5817 D4 SDA D5 1N5817 1N5817 S/KS(1) S/KS(2) S/KS(3) S/KS(4) S/KS(5)
PIN_AV8 R7
R13
220R
R12
220R J2 SDA 1 SCL 3 READY 5 7
R17
ST BY
220R
+
32/36
ZD1 V_FIL R20 10K BZX79C6V2 C9 C8 10u/50V J17 VDD_MICRO VSS-30V GND VCC3.3V GND VCC12V GND VSS-30V
R1 10K
D1
Demonstration board schematic
C2 1N5817100nF
R2 10K
1 2 3 4 5 6 7 1A 1Y 2A 2Y 3A 3Y GN D VCC 6A 6Y 5A 5Y 4A 4Y 1 ICCDAT A 2 3 ICCCLK 4 5 6 7 8 9 10
14 13 12 11 10 9 8
1 2 3 4 5 6 7
ICC CONNECTION POW ER CONNECTORS
C4 R6 4.7K R9 1K LD4 R21 220R LED1 U3 74V1G02S VCC3.3V Q2 2ST F1360
Figure 54. Schematic page 2
F1
R8
100uF 50V
+
470R
1 1A 1B VCC 2
5
S4 S6 S7 S8
MENU/SET UP DOW N RECORD S9 ST ANDBY S10 NEXT /FF S11 PREV/RR S12 S13 ST OP OPEN/CLOSE S14 PLAY/PAUSE
KEY1 KEY2
V_FIL VCC3.3V
MUT E
MUT E
R14
3 GN D 1Y
4
Q1 2ST F1360
R23 10K
R24 10K
1
Q4 BZ1 S5 MUT E 2ST F1360
F2
C6 10uF R22 10K
FILAMENT DRIVING CIRCUIT
BUZZER
MUTE CIRCUIT
VCC3.3V
S1 U6 M24C01-W MN
PIN_AV8
1 E0 E1 E2 VSS SD A 5 SC L 6 WC 7
SCL
VCC
8
10K
2 3 4
IR
LED2
LD1
J5 MHOLE 1 J6 MHOLE 1 J7
SCH
LED4
1 J8
D6
1N5817
EEPROM CIRCUIT
1
MHOLE MHOLE J15
LD2
FRONT PANEL KEYS
2 4 6 8
ST BY MUT E IRQ_N/SQW
ST BY
LD3
1
MH J16OLE T itle
LEDS & SW ITCH
1
PAGE2
UM0440
SIGNAL & POW ER HEADERS
MHOLE
Size B
Document Number ST Microelectronics Pvt. Ltd.
UM0440
Bill of materials
Appendix C
Table 2.
Bill of materials
Bill of materials
Manufacturer's /supplier's ordering code / orderable part number
Designator Qty
Reference
Value / generic part number
Package
Manufacturer/ supplier
U2 U5 U6 U4 U1 U3 VFD1 JD1 Q1,Q2,Q4 Q3 IR1 D1,D2,D3, D4,D5,D6 OPEN/ CLOSE MUTE STANDBY PIN_AV8 PLAY/ PAUSE NEXT/FF PREV/RR
1 1 1 1 1 1 1 1 3 1 1 6 1 1 1 1 1 1 1
STFPC320 front panel controller Microcontroller EEPROM (I2C protocol) Voltage Regulator Hex Inverter NOR Gate Dual Input VFD display Zener diode (6.2 V) NPN Transistor PNP Transistor IR Transceiver (36 kHz) Diode Push-button switches Push-button switches Push-button switches Push-button switches Push-button switches Push-button switches Push-button switches
STFPC320BTR ST72F325K4T6 M24C01-WMN KF40BD 74VHC14MTR 74V1G02S FUTABA 11 MT -141NK BZX796V2 2STF1360 STD790AT4 TSOP31236 1N5817
TQFP52 TQFP 32 SO 8 SO-8 SO-16 SOT23-5L Through hole Through hole SOT - 89 DPAK (TO 252) DO41 4-leg Through-hole (Push-4) 4-leg Through-hole (Push-4) 4-leg Through-hole (Push-4) 4-leg Through-hole (Push-4) 4-leg Through-hole (Push-4) 4-leg Through-hole (Push-4) 4-leg Through-hole (Push-4)
STMicroelectronics STFPC320BTR STMicroelectronics ST72F325K4T6 STMicroelectronics STMicroelectronics STMicroelectronics STMicroelectronics FUTABA Any STMicroelectronics STMicroelectronics VISHAY STMicroelectronics Farnell Farnell Farnell Farnell Farnell Farnell Farnell M24C01WMN6TP KF40BD-TR 74VHC14MTR 74V1G02STR FUTABA 11 MT -141NK BZX796V2 2STF1360 STD790AT4 TSOP31236 1N5817 535-916 535-916 535-916 535-916 535-916 535-916 535-916
33/36
Bill of materials Table 2. Bill of materials (continued)
UM0440
Designator Qty
Reference
Value / generic part number
Package
Manufacturer/ supplier
Manufacturer's /supplier's ordering code / orderable part number 535-916 535-916 535-916 535-916 535-916 535-916 926-875 244-2018
RECORD MENU/SET UP DOWN + BZ1 Y1
1 1 1 1 1 1 1 1
Push-button switches Push-button switches Push-button switches Push-button switches Push-button switches Push-button switches DC-Buzzer Cr ystal for STFPC320 32.768 kHz Cr ystal for ST72F325K4T6 16 MHz LED (green) LED (red) LED (yellow) LED (blue) Power connector Signal and power headers ICC Connector ICC Jumper
4-leg Through-hole (Push-4) 4-leg Through-hole (Push-4) 4-leg Through-hole (Push-4) 4-leg Through-hole (Push-4) 4-leg Through-hole (Push-4) 4-leg Through-hole (Push-4)
Farnell Farnell Farnell Farnell Farnell Farnell Farnell
SMT ( Surface Mount)
RS Components
Y2 LD1 LD2 LD3 LD4 J1 J2 J3 JP4 R1,R2,R7, R11,R18, R20,R22, R23,R24, R27,R31 R12,R13, R17,R21, R30 R5,R9
1 1 1 1 1 1 1 1 1
SS4 Through-hole Through-hole Through-hole Through-hole 7 way connector SIP-8 (berg strip) Header 5x2/IDC10B SIP-2 (berg strip)
Jauch Quartz Farnell Farnell Farnell Farnell RS Components Local Farnell Any
Q 16.0-SS4-2530/30 322-570 322-544 322-568 325-4616 483-8512
1106782
11
Resistor10 k
0805
Any
5 2
Resistor220 Resistor-1 k
0805 0805
Any Any
34/36
UM0440 Table 2. Bill of materials (continued)
Revision history
Designator Qty
Reference
Value / generic part number
Package
Manufacturer/ supplier
Manufacturer's /supplier's ordering code / orderable part number
R3,R4 R6,R25,R26 R8 R10 R5 R14 R15,R16 R19,R28, R29 C1,C3,C19, C20 C2,C 5,C7, C9,C11, C13,C16, C17 C6,C12, C14,C10 C15 C18
2 3 1 1 1 1 2 3 4
Resistor10 Resistor4.7 k Resistor-470 Resistor-33 k Resistor-2.7 k Resistor-330 Resistor-18 k Resistor-100 Capacitor-25 pF
0805 0805 0805 0805 0805 0805 0805 0805 0805
Any Any Any Any Any Any Any Any Any
8
Capacitor100 nF Capacitor10 F/25 V (tantalum) Capacitor2.2 F Capacitor10 nF Capacitor10 F/50 V (Tantalum) Capacitor100 F/50 V
0805
Any
4
Tantalum
Any
1 1
0805 0805
Any Any
C8
1
Tantalum
Any
C4
1
SMD - Elecrolytic
Any
5
Revision history
Table 3.
Date 26-Sep-2007
Document revision history
Revision 1 First issue Changes
35/36
UM0440
Please Read Carefully:
Information in this document is provided solely in connection with ST products. STMicroelectronics NV and its subsidiaries ("ST") reserve the right to make changes, corrections, modifications or improvements, to this document, and the products and services described herein at any time, without notice. All ST products are sold pursuant to ST's terms and conditions of sale. Purchasers are solely responsible for the choice, selection and use of the ST products and services described herein, and ST assumes no liability whatsoever relating to the choice, selection or use of the ST products and services described herein. No license, express or implied, by estoppel or otherwise, to any intellectual property rights is granted under this document. If any part of this document refers to any third party products or services it shall not be deemed a license grant by ST for the use of such third party products or services, or any intellectual property contained therein or considered as a warranty covering the use in any manner whatsoever of such third party products or services or any intellectual property contained therein.
UNLESS OTHERWISE SET FORTH IN ST'S TERMS AND CONDITIONS OF SALE ST DISCLAIMS ANY EXPRESS OR IMPLIED WARRANTY WITH RESPECT TO THE USE AND/OR SALE OF ST PRODUCTS INCLUDING WITHOUT LIMITATION IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE (AND THEIR EQUIVALENTS UNDER THE LAWS OF ANY JURISDICTION), OR INFRINGEMENT OF ANY PATENT, COPYRIGHT OR OTHER INTELLECTUAL PROPERTY RIGHT. UNLESS EXPRESSLY APPROVED IN WRITING BY AN AUTHORIZED ST REPRESENTATIVE, ST PRODUCTS ARE NOT RECOMMENDED, AUTHORIZED OR WARRANTED FOR USE IN MILITARY, AIR CRAFT, SPACE, LIFE SAVING, OR LIFE SUSTAINING APPLICATIONS, NOR IN PRODUCTS OR SYSTEMS WHERE FAILURE OR MALFUNCTION MAY RESULT IN PERSONAL INJURY, DEATH, OR SEVERE PROPERTY OR ENVIRONMENTAL DAMAGE. ST PRODUCTS WHICH ARE NOT SPECIFIED AS "AUTOMOTIVE GRADE" MAY ONLY BE USED IN AUTOMOTIVE APPLICATIONS AT USER'S OWN RISK.
Resale of ST products with provisions different from the statements and/or technical features set forth in this document shall immediately void any warranty granted by ST for the ST product or service described herein and shall not create or extend in any manner whatsoever, any liability of ST.
ST and the ST logo are trademarks or registered trademarks of ST in various countries. Information in this document supersedes and replaces all information previously supplied. The ST logo is a registered trademark of STMicroelectronics. All other names are the property of their respective owners.
2007 STMicroelectronics - All rights reserved STMicroelectronics group of companies Australia - Belgium - Brazil - Canada - China - Czech Republic - Finland - France - Germany - Hong Kong - India - Israel - Italy - Japan Malaysia - Malta - Morocco - Singapore - Spain - Sweden - Switzerland - United Kingdom - United States of America www.st.com
36/36
Document Number: 13619