NEWS
 

STMicroelectronics Releases Single-Chip SXGA Camera Module for Mobile Phones

Super-integrated imaging solution delivers best-in-class performance and flexibility for high-volume mobile applications

SXGA STMicroelectronics Releases Single-Chip Geneva, February 10,2006 - STMicroelectronics (NYSE: STM), a world leader in CMOS imaging technology and the largest supplier of camera modules for mobile phones in 2005*, has introduced its latest single-chip 1.3-Megapixel (SXGA) camera subsystem for high-volume mobile applications. Integrating a CMOS sensor with a digital image processor and analog system functions in a tiny package, ST’s VS6624 meets customer requirements for cost-effective, all-in-one mobile imaging solutions with maximum design-in flexibility.

“ST’s vertically integrated supply chain, unique in this market, allows us to control all steps in the design and manufacturing process, resulting in highly optimized cost and excellent image quality,” said Jean-Yves Gomez, Group Vice President and General Manager of ST’s Imaging Division. “Our latest all-in-one SXGA camera module benefits from ST’s advanced optical packaging, world-class image processing, and System-on-Chip integration expertise.”

The VS6624 camera module integrates a 1/3.7-inch optical-format sensor with an active pixel array of 1280 x 1024 (SXGA), using ST’s advanced 3.0 µm pixel design. ST’s latest developments in pixel defect correction, sharpness enhancement, gamma correction, and color space conversion ensure that the embedded Image Signal Processor (ISP) delivers outstanding picture quality. Advanced anti-vignetting algorithms and automatic white-balance control support top-notch color rendition in varying light conditions.

The device produces an industry-standard digital video stream at full SXGA resolution at up to 15 frames per second (fps), while its fully flexible image-scaling capability optimizes data for display in non-native resolution settings. The VS6624 also offers a low-power video mode, supporting 30 fps at VGA resolution.

The VS6624 couples excellent image quality with small space requirements and high integration flexibility. It is housed in a tiny 8 x 8 x 6 mm Small Optical Package (SmOP2), with footprint further reduced by embedding passives in the module. To enable the best fit for their end application, customers can choose between a flex-cable package and a tape-and-reel variant, compatible with a range of industry-standard hardware sockets.

In addition to mobile phones, the VS6624 camera module can be used in a wide range of portable devices such as PDAs, mobile gaming platforms, and videophones.

Engineering samples are available now, with the volume production scheduled for the end of Q1 06. Unit pricing is $8.50 in quantities up to 50,000 pieces. The device is available in two package options, mounted on a 20-way flex cable (VS6624POL5) or in Tape-And-Reel (VS6624Q0KP).

VS6624 Block


About ST’s Home, Personal, Communication Group (HPC)
STMicroelectronics is a world-leading supplier of comprehensive solutions for the converging segments of home entertainment, communication, and connectivity. ST’s HPC product offering encompasses a whole range of applications in the digital consumer market, including set-top box, DVD, TV, and audio; a wide array of solutions for personal multimedia, from application processors to energy management, mobile imaging, and wireless connectivity; and a full spectrum of display ICs and devices for wireless and wireline network infrastructures.

* Source: Prismark Partners LLC


About STMicroelectronics
STMicroelectronics is a global leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivalled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio and strategic partners positions the Company at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence markets. The Company's shares are traded on the New York Stock Exchange, on Euronext Paris and on the Milan Stock Exchange. In 2004, the Company's net revenues were $8.76 billion and net earnings were $601 million. Further information on ST can be found at www.st.com.
Information last updated Jan 2005





Should you require more information, please select the appropriate contact from the "Related Topics" menu.