![]() | ||
|
| ||
STMicroelectronics Launches New Series of AC Switches For Home Appliances
| ||
The 600V-rated ACS family of switches is built with ST’s proprietary Application Specific Devices (ASD) process technology, which enables the integration of both over-voltage protection circuitry, and RC-snubber external components. The ACS family helps users save space within electronic boards while meeting the requirements of the latest home-appliance energy-saving and Electromagnetic Compatibility (EMC) standard for testing and measurement techniques such as IEC 61000-4-5. An evolutionary advance over the previous ACS102-5Tx and ACS108-5Sx, the new ACS102-6Tx and ACS108-6Sx switches include improved static and dynamic characteristics. Among these, the latching and holding current levels have been reduced by 50%, allowing a more optimized gate pulse-control mode, especially in case of lower power rated loads, thus drastically reducing power consumption. The switching capabilities and the electrical noise immunity have been also improved by about 15% as compared to the previous version. Other major benefit of the recently introduced ACS devices is the crowbar structure, which starts to protect the system at a higher voltage level than the previous version. As a result, the devices’ robustness has been re-qualified to enable the switches to safely sustain a higher level of energy. Designers using the new ACSes will be able to cut the cost of their appliances by reducing component count up to 80% and by avoiding external over-voltage suppressors. Appliance design will also be simplified by enabling the ACSes to be directly driven from microcontrollers. The ACS102 is available in both TO-92 and SO-8 ECOPACK® packages, while the ACS108 is assembled in TO-92 and SOT-223 ECOPACK® packages. In production now, the ACS102 and ACS108 cost $0.23 and $0.25, respectively, in 10,000 unit quantities. Further information on ST’s family of AC switches is available at: www.st.com/thyristors Click here for the high-resolution photo
|
| ||||||||||||||||||||
| |||||||||||||||||||||