NEWS
 

Lighting Applications to Benefit from High-Efficiency Power MOSFET from STMicroelectronics

Click for larger image Geneva, December 05,2006 - STMicroelectronics (NYSE: STM), one of the world’s leading power semiconductor manufacturers, today introduced the first member of a new power MOSFET family. The new family allows customers to drastically reduce conduction losses and increase efficiency and reliability of their lighting applications by achieving very low ON-resistance and excellent dynamic and avalanche characteristics.

Continuous requests from the market for higher power density and lower cost in commercial lighting applications has pushed semiconductor manufacturers to drive device optimization to the limit. The new STD11NM60N, benefiting from the second generation of ST’s proprietary MDmeshTM technology, provides such optimization with a maximum RDS (ON) of 450 mOhm. The device’s resistance value is reduced by up to 55% compared to the previous MDmesh technology, without sacrificing tight control of its temperature dependence.

In addition to substantially reducing ON-state losses by minimizing the resistance value, the 600V device features an energy-optimized driver circuit which enables the MOSFET to drive higher currents at a lower VGS(th) (Voltage Gate Threshold). In fact, keeping the same threshold spread (2V), the range of VGS used to drive the device has been lowered, thus optimizing the drive and ensuring high noise immunity that prevents the circuit from switching on unintentionally.

The STD11NM60N features an excellent diode dv/dt capability as well as good avalanche performance allowing customers to keep operating temperatures within the typical working range. As a result of the very low conduction losses and reduced power dissipation, the device also helps customers cut heat-sink dimensions saving significant space board.

The small size of the chip, housed in very tiny DPAK/IPAK and TO-220FP packages, make it particularly suited to lighting applications such as High Power Factor electronic ballasts and High Intensity Discharge (HID) lamp electronic ballasts.

The STD11NM60N is available in volume now. Pricing is $0.90 in quantities of 10,000 pieces.

Technical Note
The outstanding performance of ST’s MDmeshTM (Multiple Drain meshTM) technology is due to an innovative drain structure in which the drain is implemented as an array of partitions, with vertical p-type strips, as extension of the body, aligned with the thin, horizontal n-type source strips. In the new generation of MDmesh technology, MDmesh II, further enhancements of the p-strip array have delivered a reduction of up to 55% in the RDS (ON) resistance value compared to the previous MDmesh generation, without sacrificing tight control of its temperature dependence.

Further information is available at www.st.com/pmos

Click here for the high-resolution photo


About STMicroelectronics
STMicroelectronics is a global leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivalled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio and strategic partners positions the Company at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence markets. The Company's shares are traded on the New York Stock Exchange, on Euronext Paris and on the Milan Stock Exchange. In 2005, the Company's net revenues were $8.88 billion and net earnings were $266 million. Further information on ST can be found at www.st.com.
Information last updated Jan 2006




MDmeshTM is a registered trademark of STMicroelectronics.


Should you require more information, please select the appropriate contact from the "Related Topics" menu.