NEWS
 

STMicroelectronics Showcases Infotainment, Navigation, and Safety Solutions at ITS London

Broad range of integrated circuit technologies demonstrated at 13th Intelligent Transport Systems World Congress

Geneva, October 06,2006 - STMicroelectronics (NYSE: STM), one of the world’s leading suppliers of integrated circuits for automotive systems, and recognized as a major player in the automotive GPS market, is to demonstrate a broad range of leading-edge solutions for in-vehicle entertainment, information, and safety applications at the 13th World Congress on Intelligent Transport Systems, held in London from 9 to 12 October. A mix of working and static demonstrations will showcase some of ST’s infotainment, GPS and imaging technologies, as well as both existing and prototype automotive products.

Navigation systems shown at ITS 2006 include a working prototype using ST’s NaviFlex platform – announced at ITS 2005 in San Francisco – and based on a Nomadik™ Application Processor, with ST’s GPS chipset, software platform, and reference design. NaviFlex is a complete Nomadik-based platform for in-car infotainment that targets two main markets: Car Navigation and Infotainment (NaviFlex-PRO), and Portable Navigation Devices (Naviflex-PNE platform).

A display shows GPS System-on-Chip solutions, including the STA2051 and ST’s new high-performance embedded-Flash single-chip baseband devices, and the STA2056 genuine one-chip system with on-board RF. ST has been selected by the Galileo Joint Undertaking – overseeing Europe’s global navigation satellite system – as a Prime Contractor and chipset provider for the GR-POSTER (Galileo-Ready POSitioning TERminal) program for mass market Galileo terminal development. All ST GPS chipsets will be upgraded to be Galileo-Ready.

The recently announced ADR (Advanced Digital Radio) chipset, created in collaboration with Blaupunkt, can tune in to all the current analog radio services worldwide, as well as to the new digital radio services. Combining two of ST’s TDA7528 RF front-end ICs with an STA3005 back-end chip, the solution delivers excellent sound processing and equalization performance, even in difficult signal conditions, while reducing the workload on the radio’s main microprocessor.

In-car mobile TV will be demonstrated using a working prototype, also in cooperation with Blaupunkt, that uses the T-DMB (Terrestrial Digital Multimedia Broadcasting) system, which is based on the DAB (Digital Audio Broadcasting) standard and infrastructure already operating in many European countries, including the UK. The solution is based on ST’s powerful but power-efficient Nomadik™ mobile multimedia application processor.

Satellite digital radios from leading manufacturers that use ST’s market-leading receiver and tuner ICs will be on display. For terrestrial digital radio, a prototype of a DRM (Digital Radio MondialeTM) receiver created by ST in cooperation with Kenwood and Fraunhofer IIS (Fraunhofer Institute for Integrated Circuits) will demonstrate ST’s broad capability in this field. The receiver design is expected to lead on to the development of a low-power ASIC for DRM applications in radios and PDAs.

A working automotive Media Center demonstration – with disk drive (HDD), DVD player and USB interfaces – is based on the STi710x family, which includes the world’s first single-chip H.264/AVC and VC-1 decoder; it includes wired and wireless links for PCs and smart phones.

Safety and security systems are supported by a live demonstration of 3-axis accelerometers using ST’s MEMS (Micro-Electro-Mechanical Systems) technology, with sensors detecting movement as inclination or acceleration. Applications shown include anti-theft systems for wheeled vehicles and anti-tamper systems for containers, and inputs for adaptive lighting.

The VS6x24 family of color digital cameras combines small physical size with low power consumption. They integrate a high-sensitivity pixel array, fully-featured digital image processing and camera control functions into a single die. With multiple resolutions and standard output formats (YUV, RGB or Bayer), this Imager-on-Chip (IoC) solution allows the rapid design-in of a high-quality digital camera to any system. It is shown with the x24 Camera Integration Kit (CIK) in a working demonstration of its easy evaluation and use.

A practical application of imaging technology in a vehicle environment is shown in a demonstration of a System-on-Chip (SoC) processor, the result of a joint development program between ST and Mobileye, which monitors pedestrians and lane discipline in real-time using a video stream from a single CMOS camera.

The exhibition of the 13th World Congress on Intelligent Transport Systems runs from 9th to 12th October, 2006, at ExCeL London. More details at www.itsworldcongress.com


About STMicroelectronics
STMicroelectronics is a global leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivalled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio and strategic partners positions the Company at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence markets. The Company's shares are traded on the New York Stock Exchange, on Euronext Paris and on the Milan Stock Exchange. In 2005, the Company's net revenues were $8.88 billion and net earnings were $266 million. Further information on ST can be found at www.st.com.
Information last updated Jan 2006





Should you require more information, please select the appropriate contact from the "Related Topics" menu.