New DAC offers high audio quality with on-chip power management enabling reduced footprint and direct connection to battery
|
Geneva,
January 17,2008 -
STMicroelectronics (NYSE: STM), a world leader in mobile multimedia, today announced a very high-performance 24-bit audio DAC (digital-to-analog converter) that offers 103dB dynamic range across the entire audio path. Aimed at the mobile music market, the new STw5200 is available in small TFBGA and VFQFPN packages, and soon, in a tiny 2.6 x 2.6mm WLCSP. Simplifying the system design, the DAC can also be directly connected to the battery.
The new DAC, offering Line and Headset outputs, meets the increasing demand for higher audio quality from mobile music applications and is ideal for any mobile phone platform where audio quality needs to be boosted to a Hi-Fi level. Easy system implementation, minimum bill of materials (BOM), and a very small footprint are ensured by integrated power management, which eliminates the need for an external voltage regulator, and by the built-in 50mW ‘true-ground’ headset amplifier, which operates without coupling capacitors.
The STw5200 extends ST’s audio DAC and ADC family, with enhanced audio performance. The device’s high level of integration is made possible by ST’s leading-edge 0.13-micron analog CMOS process.

Samples of the STw5200 are available now to lead customers, with volume production planned for March 2008. The DAC is priced at $1.60 in quantities of 1000 units. The chip is packaged in a 4 x 4 x 1.2mm TFBGA40, with 0.5mm ball pitch, and a 7 x 7 x 1mm VFQFPN44, with 0.5mm pitch. A 2.6 x 2.6 x 0.65mm WLCSP36 packaged version, with 0.4mm ball pitch, is planned for introduction in Q3 2008.
Click here for the high-resolution photo
About STMicroelectronics
STMicroelectronics is a global leader in developing and delivering
semiconductor solutions across the spectrum of microelectronics
applications. An unrivalled combination of silicon and system
expertise, manufacturing strength, Intellectual Property (IP)
portfolio and strategic partners positions the Company at the
forefront of System-on-Chip (SoC) technology and its products play a
key role in enabling today's convergence markets. The Company's
shares are traded on the New York Stock Exchange, on Euronext Paris
and on the Milan Stock Exchange. In 2006, the Company's net revenues
were $9.85 billion and net earnings were $782 million. Further information on ST
can be found at www.st.com.
Information last updated Jan 2007
|
|
|
|