NEWS
 

High Junction-Temperature TRIACs from STMicroelectronics Enable Smaller Heatsinks and Higher Power Density

New HiTj TRIAC series needs no parameter derating up to 150 degrees C junction temperature, and delivers top high-temperature performance for appliance AC loads

Click for larger image Geneva, February 21,2008 - STMicroelectronics (NYSE: STM) today announced a new series of high-temperature TRIACs, which maintain full specified performance up to a junction temperature of 150 degrees C, and which deliver outstanding turn-off capability – ideal for appliance motor-control applications, in particular – at their maximum temperature. The high-junction-temperature TRIACs will enable manufacturers to lower their costs by using considerably smaller heatsinks, and also allow the end product to benefit from more reliable operation in hot environments.

The use of conventional TRIACs, which are specified at 125 degrees C junction temperature, can cause a loss of control of the AC load in environments above this temperature, which can lead to hazardous application behavior, due to device parameter derating above 125 degrees C. However, ST’s new HiTj Snubberless™ series requires no derating of any of its parameters up to the maximum junction temperature, and, in fact, achieves a turn-off performance at 150 degrees C, which is three to four times better than normal. In addition, the TRIACs deliver high-noise immunity of up to 1500V/microsecond. Further cost savings are possible for manufacturers through the elimination of RC snubber circuits and noise filters.

The TRIACs are ideal for use in universal motor-control applications, such as vacuum cleaners, washing-machine drum motors, and industrial drives; in hot environments such as cookers, ovens, kitchen hobs and coffee machines; and for achieving higher power density on PCBs, for heater and high-power motor control. They can also replace conventional TRIACs in closed environments where the ambient temperature is too high.

The HiTj TRIAC series is produced in TO-220AB, TO-220AB insulated (ceramic), and in D2PAK surface-mount packages, for maximum versatility. They are all 600V devices, with current ratings of 8A, 10A, 12A, 16A and 20A. The sensitivity range offered today is 35mA to 50mA, and will soon be extended with 10mA devices.

The devices are available now in volume production, priced from $0.50 to $1.00 in 1000-unit quantities.

Datasheets:

T835H
T850H
T1035H
T1050H
T1235H
T1250H
T1635H
T1650H
T2035H
T2050H

 Click here for the high-resolution photo


About STMicroelectronics
STMicroelectronics is a global leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivalled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio and strategic partners positions the Company at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence markets. The Company's shares are traded on the New York Stock Exchange, on Euronext Paris and on the Milan Stock Exchange. In 2007, the Company's net revenues were $10.0 billion. Further information on ST can be found at www.st.com.
Information last updated Jan 2008





Should you require more information, please select the appropriate contact from the "Related Topics" menu.