NEWS
 

STMicroelectronics Innovates Integrated Protection ICs Enabling Smaller, Sleeker Power-over-Ethernet Equipment

First integrated device providing IEC 61000-4-5 surge protection for PoE applications saves 55 percent of space consumed by conventional protection circuitry

Click for larger image Geneva, June 29,2009 - Power over Ethernet (PoE), or IEEE 802.3at, is the industry standard enabling devices such as Voice-over-IP (VoIP) phones, wireless-LAN access points, RFID tag readers, sensors, or cameras to connect into a network without also requiring a nearby wall outlet for power. This enhances convenience and flexibility for end users, and also reduces equipment costs, as no external AC/DC power adapter is required. In 2008, VDC Research Group predicted that annual shipments of PoE-enabled Ethernet switches will increase to over 132 million ports by 2012.

STMicroelectronics (NYSE: STM), a world leader in protection ICs, has simplified the design of equipment for powering devices connected to an Ethernet network by introducing an integrated surge-protection IC that meets Power-over-Ethernet specifications and protects against high-voltage surges, including electrostatic discharge (ESD). ST’s PEP01-5841 protection IC is used in Power Sourcing Equipment (PSE), such as PoE-enabled Ethernet switches or hubs, which drive the specified 48V supply onto the Ethernet cable.

The PoE power-supply circuitry in the Ethernet hub or switch can withstand transients on the power lines of up to 100V. Extra protection is necessary to prevent very high voltage surges, such as ESD or EOS, from damaging the power supply. Discrete components are usually used to clamp surges to a voltage below 121V (when specified), but the PEP01-5841 integrates a 100V clamping  protection device and filtering capacitors for up to four PoE outputs in a single 5 x 6mm component. This simplifies design and saves up to 55 percent of printed-circuit-board space.

The PEP01-5841 is the first device providing 1kV surge protection as specified by IEC 61000-4-5 that also has a clamping voltage compatible with the 100V PSE controller. ESD protection satisfies worldwide standards including IEC 61000-4-2 and MIL-STD-883 Method 3015.

The PEP01-5841 is available immediately, in the industry-standard SO-8 package, priced at $0.25 in quantities of 10,000 pieces.

Click here for the high-resolution photo


About STMicroelectronics
STMicroelectronics is a global leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivalled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio and strategic partners positions the Company at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence markets. The Company's shares are traded on the New York Stock Exchange, on Euronext Paris and on the Milan Stock Exchange. In 2008, the Company's net revenues were $9.84 billion. Further information on ST can be found at www.st.com.
Information last updated Jan 2009





Should you require more information, please select the appropriate contact from the "Related Topics" menu.